Overland Park, Kan. SPX Cooling Technologies, Inc., a full-line, full-service industry leader in the design and manufacture of evaporative cooling towers and air-cooled heat exchangers, has issued a video series about the advantages of using genuine Marley® parts. The three-part series, hosted by SPX Product Manager Jerome Jennings, includes a video on: 1) Marley Geareducer® gear drives, 2) Marley driveshafts, and 3) Marley fan blades.

In video one, Jennings covers the benefits of using the Marley Geareducer gear drive. Some advantages discussed include the greater surface area and larger oil ports compared to other manufacturers’ gearboxes, the long lifecycle of its bearings and more.

Jennings addresses the Marley Comp-DS cooling tower driveshaft in the second video. The key aspects of the Marley Comp-DS driveshaft include the differentiated low maintenance design of its hub, tube and flange assembly, and the use of carbon fiber in the driveshaft’s flex element, which is lighter weight yet more durable than fiberglass.

Marley fan blades also feature unique characteristics. As Jennings discusses in the third video of the series, infused pigmentation, instead of a painted layer that can flake or crack over time, protects Marley fan blades from sunlight or moisture. Other positives covered in the video include the Marley blades’ single-piece construction, high-strength wide-shank design, and efficient flared blade-tip design.

Together, these three videos provide an overview of the benefits customers derive from choosing Marley OEM replacement component parts for cooling towers – specifically, the robust design of the Marley Geareducer gear drive, the reliable Marley Comp-DS cooling tower driveshaft, and the efficient, well-constructed Marley fan blades.

To watch additional videos on cooling towers, components and maintenance techniques, visit: http://spxcooling.com/video.


Marley Cooling Tower Parts