featured-image
FOR IMMEDIATE RELEASE Contact: Kristin Nugent McNeil, Gray & Rice 617-367-0100, ext. 148 kristin.nugent@mgr1.com

Overland Park, KS SPX Cooling Technologies, Inc., a full-line, full-service industry leader in the design and manufacture of evaporative and air-cooled heat exchangers, and sister company, SPX Heat Transfer, LLC will showcase several innovative technologies at the Geothermal Energy Association GEOEXPO+, October 23-26, 2016, at the Sacramento Convention Center. In Booth #303, SPX Cooling Technologies will feature two new Marley® cooling tower designs. SPX Heat Transfer will feature the Ecolaire® Advanced Direct Contact Condenser (ADCC). Aftermarket services and OEM components from both companies complete the offering.

The new Marley NC Everest™ Cooling Tower offers 50% more cooling capacity than any other pre-assembled cooling tower in the world.* It offers several advantages over traditional field-erected towers for geothermal applications, including up to 60% faster delivery and field installation in about 20% of the time.* It also offers reduced onsite labor and work duration for safer assembly processes and work environment.

The new Marley Modular F400 Cooling Tower is a field-erected tower that utilizes factory-assembled modules to provide uniform quality components and faster onsite assembly. Sections of the tower are shipped just-in-time to the job site. Faster installation results in a reduced construction schedule.

The Ecolaire ADCC is licensed technology designed for geothermal power that condenses steam directly from geothermal wells or steam flashed from hot brine. The ADCC uses a turbulent film to condense the steam. The higher thermal efficiency of the ADCC enables many benefits for a geothermal power system.

Representatives from SPX Cooling Technologies and SPX Heat Transfer will be available throughout the show to discuss products, projects and aftermarket support programs.

*Compared to other leading manufacturers.



Top

Marley Cooling Tower Parts