FOR IMMEDIATE RELEASE FOR IMMEDIATE RELEASE Contact: Jodie Klaus SPX Cooling Technologies, Inc. 913 664 7710 Jodie.klaus@spx.com SPX Cooling Technologies, Inc. announces the expansion of its Marley MD cooling tower line. Multiple enhancements have been made to this induced-draft counterflow cooling tower to give it a smaller footprint that offers layout alternatives. The Marley MD expanded line incorporates other features such as: • The CTI Certified Marley MD cooling tower comes with the Marley Ultra Quiet fan and other fan and attenuation options to meet the most stringent sound requirements. • Triple-pass inlet louvers limit the sunlight entering the collection basin reducing the potential for algae growth. Large access doors with removable block fill and other features simplify maintenance. • As an option, all collection basin parts exposed to circulating water and all basin options are made of heavy-gauge series 300 stainless steel for extra protection. • The factory-installed optional basin sweeper piping augments the filtration system to keep all equipment running smoothly. These features, along with unmatched reliability, low energy consumption and a superior water management system, make the Marley MD cooling tower the right solution for light industrial and HVAC applications.
SPX Cooling Technologies, Inc. SPX Cooling Technologies, Inc. is a leading global manufacturer of cooling towers and air-cooled condensers, providing full-service cooling solutions and supporting customers in the power generation, petrochemical, industrial, refrigeration, and heating, ventilation and air conditioning (HVAC) markets for more than 100 years. Visit http://www.spxcooling.com.


Top

Marley Cooling Tower Parts