FOR IMMEDIATE RELEASE FOR IMMEDIATE RELEASE Contact: Jodie Klaus SPX Cooling Technologies, Inc. 913 664 7710 Jodie.klaus@spx.com SPX Cooling Technologies, Inc. announces the availability of new and improved models within its Marley MH Fluid Cooler product line. These product line enhancements follow several others that were introduced earlier this year. Key features of the MH Fluid Cooler 7100 models launched in phase II include: Improved design and expanded options available in the three smallest MH Fluid Cooler box sizes Height reduction, shipping improvements and performance increases incorporated on various models Quiet Fan, Ultra Quiet Fan and Inlet Attenuation options offering significantly reduced sound levels An optional finned coil in the tower plenum enabling part-load dry operation in cold ambient conditions Expanded CTI Certification listing now including the options above, as well as optional stainless steel coils and use of aqueous glycol solutions These enhancements improve the flexibility of the Marley MH Fluid Cooler product line. The Marley MH Fluid Cooler is one of the most energy efficient closed circuit systems on the market and a great choice for closed loop industrial and HVAC applications.
SPX Cooling Technologies, Inc. SPX Cooling Technologies, Inc. is a leading global manufacturer of cooling towers and air-cooled condensers, providing full-service cooling solutions and supporting customers in the power generation, petrochemical, industrial, refrigeration, and heating, ventilation and air conditioning (HVAC) markets for more than 100 years. Visit http://www.spxcooling.com.


Top

Marley Cooling Tower Parts