FOR IMMEDIATE RELEASE FOR IMMEDIATE RELEASE Contact: Jodie Klaus SPX Cooling Technologies, Inc. 913 664 7710 Jodie.klaus@spx.com SPX Cooling Technologies, Inc. launches two new videos highlighting the proven history and superior performance of their Marley Geareducer. Recently uploaded to http://www.spxcooling.com, the videos explain the Geareducer rebuild/repair process (a part of the Marley Geareducer Solutions program) and the advantages of using a Marley OEM Geareducer. With the Marley Geareducer Solutions program, not only can customers order a new replacement gearbox for a cooling tower from SPX, a factory-trained technician can also repair the existing gearbox or rebuild a gearbox at their plant in Olathe, KS. This process is highlighted in the Rebuild/Repair Process video. As shown in the OEM Difference video, there are several critical differentiations of a Marley Geareducer. • The bearing life of a Marley Geareducer is 100,000 hours, while the competition is 50,000 hours. • Larger oil ports on each Marley Geareducer ensure maximum service life. • To ensure maximum strength, the integral pinion shaft is a single piece pinion. • Sound levels are up to 80% lower, as a result of our high quality gears. • 47% greater surface area due to many external fins the help reject heat and keep the unit running cool. To view the Marley Geareducer videos or to learn more about the Marley Geareducer Solutions program, go to http://www.spxcooling.com/en/geareducer.
SPX Cooling Technologies, Inc. SPX Cooling Technologies, Inc. is a leading global manufacturer of cooling towers and air-cooled condensers, providing full-service cooling solutions and supporting customers in the power generation, petrochemical, industrial, refrigeration, and heating, ventilation and air conditioning (HVAC) markets for more than 100 years. Visit http://www.spxcooling.com.


Top

Marley Cooling Tower Parts