FOR IMMEDIATE RELEASE
FOR IMMEDIATE RELEASE
Contact:
Jodie Klaus
SPX Cooling Technologies, Inc.
913 664 7710
Jodie.klaus@spx.com
SPX Cooling Technologies, Inc. announces the availability of new and improved models within its Marley MH Fluid Cooler product line. These product line enhancements are the first of several that will be introduced this year.
Key features of the new MHF7100 models launched in this phase include:
• Improved design and expanded options available in the three smallest MH Fluid Cooler box sizes
• Quiet Fan, Ultra Quiet Fan and Inlet Attenuation options offer significantly reduced sound levels
• An optional finned coil in the tower plenum now enables part-load dry operation in cold ambient conditions
• Expanded CTI Certification listing now includes the options above, optional stainless steel coils, and use of aqueous glycol solutions
• Various models incorporate height reduction, shipping improvements, and performance increases
These enhancements improve the flexibility of the Marley MH Fluid Cooler product line. The Marley MH Fluid Cooler is one of the most energy efficient closed circuit systems on the market and a great choice for closed loop industrial and HVAC applications.
SPX Cooling Technologies, Inc. SPX Cooling Technologies, Inc. is a leading global manufacturer of cooling towers and air-cooled condensers, providing full-service cooling solutions and supporting customers in the power generation, petrochemical, industrial, refrigeration, and heating, ventilation and air conditioning (HVAC) markets for more than 100 years. Visit http://www.spxcooling.com.
SPX Cooling Technologies, Inc. SPX Cooling Technologies, Inc. is a leading global manufacturer of cooling towers and air-cooled condensers, providing full-service cooling solutions and supporting customers in the power generation, petrochemical, industrial, refrigeration, and heating, ventilation and air conditioning (HVAC) markets for more than 100 years. Visit http://www.spxcooling.com.