FOR IMMEDIATE RELEASE FOR IMMEDIATE RELEASE Contact: Jodie Klaus SPX Cooling Technologies, Inc. 913 664 7710 Jodie.klaus@spx.com SPX OFFERS NEW, REBUILD AND REPAIR OPTIONS FOR YOUR COOLING TOWER GEARBOX Overland Park, KS, August 2012 – SPX Cooling Technologies, Inc. today announced the introduction of the Geareducer Solutions program. Not only can customers order a new replacement gearbox for a cooling tower from SPX, but now, a factory-trained technician can repair the existing gearbox or rebuild a gearbox at their plant in Olathe, KS. With the Geareducer Solutions program, you can be confident SPX has a solution regardless of your needs. New Marley® Geareducer® For over 75 years, the Marley Geareducer has set the standard for excellence in performance and durability. -Quality gears provide longer life and over 30% lower sound compared to lower class gear sets. -Bearings have twice the L10A service life for input and intermediate shafts that require half the maintenance costs. -Marley Geareducers have a 100,000-hour service interval on input and intermediate shaft bearings. Rebuilt Marley Geareducer When SPX rebuilds a gearbox, only genuine Marley OEM components are used to ensure the appearance, reliability and performance customers have come to expect from a new Marley Geareducer. -All rebuilt Marley Geareducers have a comprehensive one-year warranty that covers all components, including the seals and bearings. -Critical components and cores are stocked to meet your specific needs with short lead times. -Prior to shipment, all Marley Geareducers are factory dyno-tested under full load to ensure factory OEM specifications are met. Repaired Marley Geareducer With the Marley Geareducer repair option, a qualified SPX technician will use factory-designed tools, dies and jigs to repair the unit to meet all Marley OEM performance specifications. -During the disassembly process, measurements are made to determine the condition and setup of the gearbox and a detailed report is produced. -After re-assembly, all Marley Geareducers are factory dyno-tested under full load prior to shipment to ensure it is running at the rated torque and horsepower. -All repaired Marley Geareducers have a comprehensive one-year warranty that covers all components of the gearbox, including the seals and bearings. For more information about the Marley Geareducer Solutions program or to download the brochure, go to http://www.spxcooling.com/en/geareducer. About SPX Cooling Technologies, Inc. SPX Cooling Technologies, Inc. is a leading global manufacturer of cooling towers and air-cooled condensers, providing full-service cooling solutions and supporting customers in the power generation, petrochemical, industrial, refrigeration, and heating, ventilation and air conditioning (HVAC) markets for more than 100 years. Visit http://www.spxcooling.com. SPX Cooling Technologies and its product brands are part of SPX (NYSE: SPW), a global Fortune 500 multi-industry manufacturing company. With headquarters in Charlotte, N.C., SPX has 18,000 employees in more than 35 countries worldwide. Visit http://www.spx.com.


Top

Marley Cooling Tower Parts