FOR IMMEDIATE RELEASE FOR IMMEDIATE RELEASE Contact: Jodie Klaus SPX Cooling Technologies, Inc. 913 664 7710 Jodie.klaus@spx.com CHARLOTTE, N.C., May 30, 2013 /PRNewswire/ -- SPX Corporation (NYSE: SPW) today announced that its Thermal Equipment and Services segment has been awarded new orders for dry cooling systems for three different power plants in Indonesia, Jordan and Mexico totaling approximately $40 million. Under the terms of the contracts, SPX will provide air cooled condensers (ACC) to a 2x140 MW coal-fired power plant in Babelan, Indonesia, to the SAMRA III 140 MW add-on combined cycle power plant in Al Zarqa, Jordan, and to a 205 MW combined cycle power plant in San Luis de la Paz, Mexico. "As emerging and developed countries around the world continue to expand their energy infrastructure to meet growing demand for electricity, we continue to see demand for our highly efficient dry cooling technologies for power plants," said Gene Lowe, SPX segment president. "SPX's air cooled condensers are a popular cooling system choice for power producers operating various types of power plants in dry climates where water usage is restricted or where water is in low supply." While dry cooling technology is widely utilized for coal-fired power plants as well as combined cycle natural gas and waste incineration plants, it is also increasingly being applied in renewable energy generation including solar thermal and biomass plants. With these orders on three different continents SPX continues to demonstrate its position as a leading provider of highly innovative dry cooling technology.


Top

Marley Cooling Tower Parts