MD Revit File
The Revit product family for the Marley® MD cooling tower (“MD”) provides the basic geometry and typical pipe connections for each unit size of the product line. The product family is compatible with Revit version 2012 and later.
Conexiones de entrada
All model sizes of the MD have a single inlet connection per cell. The standard inlet location is on face A, but face B, C, or D may be alternately selected. Only one of the inlets should be connected; the others should be ignored or deleted. On models MD5006, MD5008 and MD5010, the water inlet and the motor cannot be located on the same face. The inlet size defaults to a commonly used pipe diameter for the unit size selected. Actual inlet size may vary depending on the design flow rate, and should be confirmed in the quotation.
Conexiones de salida
Three types of outlet connections are included in this product family: side suction outlet (face A), bottom outlet, and end suction outlet (face B or D). Sólo uno de los puntos de venta should be connected; the others should be ignored or deleted. Outlet size defaults to a commonly used pipe diameter for the unit size selected. Actual outlet size may vary depending on the design flow rate, and should be confirmed in the quotation. The MD has an option for a sump outlet which is not included in this model.
Motor Face
The fan motor may be configured on either face A or face C. A plenum access door is provided on the motor face to allow access to the interior mechanical equipment, drift eliminators and spray system. If an optional mechanical access platform is selected, it will be installed on the same face as the motor. On models MD5006, MD5008 and MD5010, the motor is external to the airstream and cannot be located on the same face as the water inlet.
Accesorios Opcionales
Los siguientes accesorios opcionales son parámetros seleccionables en la categoría Estructural:
Ventilador ultrasilencioso
Mechanical Access Platform on Face A
Mechanical Access Platform on Face C
Mechanical Access Platforms are only available on the motor face. Other optional accessories may alter or prevent the use of these options and/or increase the size of the unit.
Múltiples celdas
Multiple instances of the MD product family may be inserted into the Revit project for installations having multiple cells. Ensure the proper Revit model is selected, including applicable cell count, as tower height may vary depending on the number of cells in the final installation. Inline arrangements are the most common, and are characterized by face B of one cell being oriented towards face D of the next cell. Face B and face D are shorter than faces A and C. Some model sizes may also be arranged back to back, with face A of one cell oriented towards face C of the next cell. Cells arranged in this fashion must have either face A or face C open. Model sizes that can be oriented back to back can also be configured in a Quad arrangement, which is a four-cell combination of inline and back to back cells.
Los espacios estándar entre celdas de centro a centro se enumeran por tamaño de modelo en la siguiente tabla.
Espaciado de celdas de centro a centro |
||
Tamaño de la unidad |
Inline |
Back-to-Back |
MD5006 |
104.00” (2642mm) |
N/A |
MD5008 |
110.00″ (2794mm) |
N/A |
MD5010 |
146.25″ (3715mm) |
N/A |
MD5016 |
146.25″ (3715mm) |
145.875″ (3705mm) |
MD5018 |
218.25” (5544mm) |
145.875″ (3705mm) |
Liquidaciones
The mechanical access platform option shows the required clearance for a safety cage on the platform ladder. Additionally, clearance must be provided at the air inlets and air discharge for adequate air flow. The clearance requirements vary by application, but the air inlet clearance can be approximated as half of the long side of one cell, and the air discharge clearance should be three fan diameters. Also note that vertical enclosures around the cooling tower should not rise above the fan discharge, otherwise air recirculation may impact performance.
Al hacer clic en "Aceptar", acepta nuestros Términos y condiciones:
Al hacer que esta información esté disponible, SPX Cooling no presta servicios profesionales y no asume ningún deber, responsabilidad u obligación con respecto a cualquier persona que haga uso de dicha información, incluidas las modificaciones realizadas por el usuario, para el diseño de edificios y sistemas relacionados. utilizando dicha Información, o por la exactitud de dicha Información o cualquier dato resultante del uso de la misma. Esta información se proporciona "tal cual" y SPX Cooling no será responsable de ningún reclamo, demanda, lesión, pérdida, gasto o responsabilidad de ningún tipo, incluidos, entre otros, daños directos, indirectos, incidentales o consecuentes. que de alguna manera surja o esté relacionado con el uso de la Información, ya sea que dicha reclamación, pérdida, gasto o responsabilidad resulte o no directa o indirectamente de cualquier acción u omisión de SPX Cooling o sus empleados y representantes resultantes del uso de esta información.
SPX Cooling no ofrece ninguna garantía de ningún tipo, ya sea expresa o implícita, incluida, entre otras, cualquier garantía de comerciabilidad o idoneidad para un propósito particular, ni hace ninguna declaración con respecto al uso o los resultados del uso del Información en términos de su exactitud, validez, integridad, aplicabilidad o cumplimiento de cualquier código regulatorio o leyes y regulaciones gubernamentales. El uso de la Información implica algunos riesgos, y todo el riesgo en cuanto a los resultados y el rendimiento de la Información es responsabilidad del usuario.
SPX Cooling conserva el título y la propiedad de toda la Información y todas las copias de la misma y todos los demás derechos e intereses, incluidos, entre otros, patentes, derechos de autor, marcas comerciales, secretos comerciales y otros derechos de propiedad intelectual, sobre la Información y cualquier copia de la misma. . Al aceptar o utilizar esta información, el usuario acepta no usarla excepto como se establece expresamente en este documento y el usuario acepta no usar esta información para representar los productos de ningún fabricante que no sea SPX Cooling, sus empresas matrices o subsidiarias.
Excepto lo expresamente dispuesto en estos Términos de uso, ninguna parte de la Información puede copiarse, reproducirse, republicarse, cargarse, publicarse, mostrarse públicamente, codificarse, traducirse, transmitirse o distribuirse de ninguna manera a cualquier otra computadora, servidor, sitio web o otro medio para publicación o distribución o para cualquier empresa comercial, sin el consentimiento previo expreso por escrito de SPX Cooling.
Puede utilizar la información que SPX Cooling pone a disposición intencionalmente para su descarga, siempre que (1) no elimine ningún lenguaje de aviso de propiedad en todas las copias de dichos documentos, (2) utilice dicha información solo para su uso comercial interno y (3) no hará ninguna declaración o garantía adicional relacionada con dicha información.
Este Acuerdo y cualquier disputa que surja de o en conexión con este Acuerdo se regirán por las leyes del Estado de Kansas, EE. UU., sin ninguna referencia a principios de conflicto de leyes.
Los productos de SPX Cooling están sujetos a mejoras continuas. SPX Cooling se reserva el derecho de modificar el diseño, las especificaciones y los datos del producto sin previo aviso y sin incurrir en ninguna obligación.