Seite wählen

NC8400 Revit Files (Including NC Everest)

The Revit product family for the Marley NC8400 steel cooling tower provides the basic geometry and typical pipe connections for each unit size of the product line. The product family does not cover the fiberglass cased version of the NC8400 cooling tower. The product family is compatible with Revit version 2012 and later and may be downloaded at / wiederaufnehmen.

Einlassanschlüsse
The standard dual inlet connections are included in this product family. The inlet size is automatically set according to the unit size selected. The piping connected to these inlets should supply equal water flow to both inlets. The horizontal control (HC) valves option and the Marley single inlet option are not included in this model.

Auslassanschlüsse
Three types of outlet connections are included in this product family: side outlet face A, side outlet face C, and bottom outlet. Only one of the outlets should be connected; the other two should be ignored or deleted. After the inlet water flows are defined, the outlet water flow and outlet diameters are calculated automatically. Side outlets are not applicable to NC8422 models. The NC8400 has an option for a sump outlet which is not included in this model.

Optionales Zubehör
Die folgenden optionalen Zubehörteile sind in der Kategorie Strukturell wählbare Parameter:

  • VR (Velocity Recovery) Stack
  • Ultra Quiet Fan Option
  • Guardrail with Ladder on Face A
  • Guardrail with Ladder on Face B
  • Guardrail with Ladder on Face C
  • Guardrail with Ladder on Face D
  • Access Door Platform on Face A
  • Access Door Platform on Face C

The ladder options for faces A and C cannot be used in combination with the ladder options for faces B and D. The access door platform cannot be used on the same face as a side outlet. Other optional accessories may alter or prevent the use of these options, and some optional components can increase the size of the unit. VR (Velocity Recovery) Stack and Ultra Quiet Fan Option are not applicable to NC8422 models.

Mehrere Zellen
Multiple instances of the NC8400 product family may be inserted into the Revit model for installations having multiple cells. They must all be oriented in the same direction and positioned so the access doors on faces A and C are facing each other. There is a standard spacing between cells and an alternate wider spacing to permit the fan motor to be mounted outside the airstream. Ladders and Access Door Platforms cannot be used between cells.

Center-to-Center Spacing

Einheitsgröße

Standard

Wide

NC8401

81.75” (2076mm)

114” (2896mm)

NC8402

104.25” (2648mm)

136.5” (3467mm)

NC8403

104.25” (2648mm)

136.5” (3467mm)

NC8405

122.25” (3105mm)

154.5” (3924mm)

NC8407

146.25” (3715mm)

178.5” (3434mm)

NC8409

170.25” (4324mm)

202.5” (5144mm)

NC8410

146.25” (3715mm)

178.5” (3434mm)

NC8411

146.25” (3715mm)

178.5” (3434mm)

NC8412

170.25” (4324mm)

202.5” (5144mm)

NC8413

146.25” (3715mm)

178.5” (3434mm)

NC8414

170.25” (4324mm)

202.5” (5144mm)

NC8422

272.5” (6922mm)

321” (8153mm)

 

Freigaben
The guardrail, ladder, and access door accessories show the required clearance for these options. Additionally, clearance must be provided at the air inlets and air discharge for adequate air flow. The clearance requirements vary by application, but the air inlet clearance can be approximated as the width of the air inlet for one cell, and the air discharge clearance should be three fan diameters. Also note that vertical enclosures around the cooling tower should not rise above the fan discharge, otherwise air recirculation will impact performance.

Indem Sie auf „Zustimmen“ klicken, akzeptieren Sie unsere Allgemeinen Geschäftsbedingungen:

Die in dieser Datei bereitgestellten Produktinformationen von SPX Cooling Technologies, Inc. („SPX Cooling“) (einschließlich Design und Abmessungen) („Informationen“) dienen ausschließlich zu Informationszwecken und sind kein Ersatz für eine professionelle technische Überprüfung und Bewertung der Situation. Die endgültige Bewertung der Anwendung sollte immer von einem professionellen Ingenieur mit Zulassung im entsprechenden Ingenieurbereich vorgenommen werden. Diese Person und nicht SPX Cooling oder seine Mitarbeiter und Vertreter ist für das endgültige technische Design und die Leistung der vorliegenden Anwendung verantwortlich.

Mit der Bereitstellung dieser Informationen erbringt SPX Cooling keine professionellen Dienstleistungen und übernimmt keine Pflichten, Verantwortung oder Haftung gegenüber Personen, die diese Informationen verwenden, einschließlich aller vom Benutzer vorgenommenen Änderungen, für die Gestaltung von Gebäuden und zugehörigen Systemen, die unter Verwendung dieser Informationen erstellt wurden, oder für die Richtigkeit dieser Informationen oder aller Daten, die sich aus der Verwendung dieser Informationen ergeben. Diese Informationen werden „wie besehen“ bereitgestellt und SPX Cooling haftet nicht für Ansprüche, Forderungen, Verletzungen, Verluste, Kosten oder Haftungen jeglicher Art, einschließlich, aber nicht beschränkt auf direkte, indirekte, zufällige oder Folgeschäden, die in irgendeiner Weise aus der Verwendung der Informationen entstehen oder damit in Zusammenhang stehen, unabhängig davon, ob diese Ansprüche, Forderungen, Verluste, Kosten oder Haftungen direkt oder indirekt aus Handlungen oder Unterlassungen von SPX Cooling oder seinen Mitarbeitern und Vertretern resultieren, die sich aus der Verwendung dieser Informationen ergeben.

SPX Cooling übernimmt keinerlei ausdrückliche oder stillschweigende Gewährleistungen oder Garantien, einschließlich, aber nicht beschränkt auf Gewährleistungen der Marktgängigkeit oder Eignung für einen bestimmten Zweck, und macht keine Zusicherungen hinsichtlich der Verwendung oder der Ergebnisse der Verwendung der Informationen hinsichtlich ihrer Genauigkeit, Gültigkeit, Vollständigkeit, Anwendbarkeit oder Einhaltung von Vorschriften oder staatlichen Gesetzen und Vorschriften. Die Verwendung der Informationen birgt gewisse Risiken, und das gesamte Risiko hinsichtlich der Ergebnisse und Leistung der Informationen liegt in der Verantwortung und Haftung des Benutzers.

SPX Cooling behält das Eigentum an allen Informationen und allen Kopien davon sowie alle anderen Rechte und Ansprüche, einschließlich, aber nicht beschränkt auf Patente, Urheberrechte, Marken, Geschäftsgeheimnisse und andere Rechte an geistigem Eigentum, an den Informationen und allen Kopien davon. Durch die Annahme oder Verwendung dieser Informationen erklärt sich der Benutzer damit einverstanden, diese Informationen nur wie hierin ausdrücklich dargelegt zu verwenden, und der Benutzer erklärt sich damit einverstanden, diese Informationen nicht zu verwenden, um die Produkte anderer Hersteller als SPX Cooling, seiner Muttergesellschaften oder Tochtergesellschaften darzustellen.

Sofern in diesen Nutzungsbedingungen nicht ausdrücklich etwas anderes vorgesehen ist, darf kein Teil der Informationen ohne die vorherige ausdrückliche schriftliche Zustimmung von SPX Cooling kopiert, reproduziert, erneut veröffentlicht, hochgeladen, gepostet, öffentlich angezeigt, kodiert, übersetzt, übertragen oder in irgendeiner Weise an einen anderen Computer, Server, eine Website oder ein anderes Medium zur Veröffentlichung oder Verteilung oder für gewerbliche Unternehmen verteilt werden.

Sie dürfen die von SPX Cooling absichtlich zum Herunterladen bereitgestellten Informationen verwenden, vorausgesetzt, dass Sie (1) in allen Kopien dieser Dokumente keine Eigentumshinweise entfernen, (2) diese Informationen nur für Ihre internen Geschäftszweck verwenden und (3) keine zusätzlichen Zusicherungen oder Gewährleistungen in Bezug auf diese Informationen abgeben.

Diese Vereinbarung und alle Streitigkeiten, die sich aus oder im Zusammenhang mit dieser Vereinbarung ergeben, unterliegen den Gesetzen des US-Bundesstaates Kansas, ohne Bezugnahme auf Kollisionsnormen.

Die Produkte von SPX Cooling unterliegen ständigen Verbesserungen. SPX Cooling behält sich das Recht vor, Produktdesign, Spezifikationen und Daten ohne Vorankündigung und ohne Verpflichtung zu ändern.

de_DE