Seite wählen

Quadraflow Revit Files

The Revit product family for the Marley® Quadraflow® cooling tower (“QF”) provides the basic geometry and typical pipe connections for each unit size of the product line.  The product family is compatible with Revit version 2012 and later, and may be downloaded at / wiederaufnehmen.

Einlassanschlüsse
The inlet connection(s) for all Quadraflow models is a hole and grommet in the top deck sized to accept insertion of an appropriately sized inlet pipe.  The quantity and size of inlet connections varies depending on model size.  21000 and 22000 models have one 8” inlet per cell, located on any of the four corners.  23000 models whose design flow is 2025 gpm per cell or less may use a single 10” inlet.  Above 2025 gpm per cell, two 8” inlets are required, located 180 degrees apart.  24000 models use two 10” inlets per cell, located 180 degrees apart.  Locating an inlet riser directly behind the motor is allowed, but not recommended due to restrictions placed on motor access and removal.

 Auslassanschlüsse
21000, 22000 and 23000 models use a bottom sump outlet.  24000 models use a side sump outlet.  Outlet connection size defaults to a commonly used pipe diameter for the unit size selected.  Actual outlet size may vary depending on the design flow rate and outlet location, and should be confirmed in the quotation.

Mehrere Zellen
Multiple instances of the Quadraflow product family may be inserted into the Revit project for installations having multiple cells.  Two cell installations may be installed using either a square pattern or a diamond pattern.  Multi-cell installations of more than two cells are typically installed using a diamond pattern – if a square pattern is used for more than two cells, the cell spacing required is greater than the spacing shown below.

Die standardmäßigen Zellabstände von Mitte zu Mitte sind nach Modellgröße in der folgenden Tabelle aufgeführt.

     

Zellabstand von Mitte zu Mitte

Einheitsgröße

Square Layout

Diamond Layout

21120

192.125” (4880mm)

181.750” (4616mm)

21220

198.125″ (5032mm)

181.750” (4616mm)

21320

203.125” (5159mm)

181.750” (4616mm)

22120

219.625” (5578mm)

205.125” (5210mm)

22220

225.625″ (5731mm)

205.125” (5210mm)

23120

258.125″ (6556mm)

230.875” (5864mm)

23220

263.125″ (6683mm)

230.875” (5864mm)

24120

345.000” (8763mm)

341.625” (8677mm)

24220

362.000” (9195mm)

341.625” (8677mm)

Freigaben
Sufficient clearance should be provided to allow safe access to the tower and its components.  Additionally, clearance must be provided at the air inlets and air discharge for adequate air flow.  The clearance requirements vary by application, but the air inlet clearance can be approximated as 6 ft., and the air discharge clearance should be at least three fan diameters.  Also note that vertical enclosures around the cooling tower should not rise above the fan discharge, otherwise air recirculation may impact performance.

Indem Sie auf „Zustimmen“ klicken, akzeptieren Sie unsere Allgemeinen Geschäftsbedingungen:

Die in dieser Datei bereitgestellten Produktinformationen von SPX Cooling Technologies, Inc. („SPX Cooling“) (einschließlich Design und Abmessungen) („Informationen“) dienen ausschließlich zu Informationszwecken und sind kein Ersatz für eine professionelle technische Überprüfung und Bewertung der Situation. Die endgültige Bewertung der Anwendung sollte immer von einem professionellen Ingenieur mit Zulassung im entsprechenden Ingenieurbereich vorgenommen werden. Diese Person und nicht SPX Cooling oder seine Mitarbeiter und Vertreter ist für das endgültige technische Design und die Leistung der vorliegenden Anwendung verantwortlich.

Mit der Bereitstellung dieser Informationen erbringt SPX Cooling keine professionellen Dienstleistungen und übernimmt keine Pflichten, Verantwortung oder Haftung gegenüber Personen, die diese Informationen verwenden, einschließlich aller vom Benutzer vorgenommenen Änderungen, für die Gestaltung von Gebäuden und zugehörigen Systemen, die unter Verwendung dieser Informationen erstellt wurden, oder für die Richtigkeit dieser Informationen oder aller Daten, die sich aus der Verwendung dieser Informationen ergeben. Diese Informationen werden „wie besehen“ bereitgestellt und SPX Cooling haftet nicht für Ansprüche, Forderungen, Verletzungen, Verluste, Kosten oder Haftungen jeglicher Art, einschließlich, aber nicht beschränkt auf direkte, indirekte, zufällige oder Folgeschäden, die in irgendeiner Weise aus der Verwendung der Informationen entstehen oder damit in Zusammenhang stehen, unabhängig davon, ob diese Ansprüche, Forderungen, Verluste, Kosten oder Haftungen direkt oder indirekt aus Handlungen oder Unterlassungen von SPX Cooling oder seinen Mitarbeitern und Vertretern resultieren, die sich aus der Verwendung dieser Informationen ergeben.

SPX Cooling übernimmt keinerlei ausdrückliche oder stillschweigende Gewährleistungen oder Garantien, einschließlich, aber nicht beschränkt auf Gewährleistungen der Marktgängigkeit oder Eignung für einen bestimmten Zweck, und macht keine Zusicherungen hinsichtlich der Verwendung oder der Ergebnisse der Verwendung der Informationen hinsichtlich ihrer Genauigkeit, Gültigkeit, Vollständigkeit, Anwendbarkeit oder Einhaltung von Vorschriften oder staatlichen Gesetzen und Vorschriften. Die Verwendung der Informationen birgt gewisse Risiken, und das gesamte Risiko hinsichtlich der Ergebnisse und Leistung der Informationen liegt in der Verantwortung und Haftung des Benutzers.

SPX Cooling behält das Eigentum an allen Informationen und allen Kopien davon sowie alle anderen Rechte und Ansprüche, einschließlich, aber nicht beschränkt auf Patente, Urheberrechte, Marken, Geschäftsgeheimnisse und andere Rechte an geistigem Eigentum, an den Informationen und allen Kopien davon. Durch die Annahme oder Verwendung dieser Informationen erklärt sich der Benutzer damit einverstanden, diese Informationen nur wie hierin ausdrücklich dargelegt zu verwenden, und der Benutzer erklärt sich damit einverstanden, diese Informationen nicht zu verwenden, um die Produkte anderer Hersteller als SPX Cooling, seiner Muttergesellschaften oder Tochtergesellschaften darzustellen.

Sofern in diesen Nutzungsbedingungen nicht ausdrücklich etwas anderes vorgesehen ist, darf kein Teil der Informationen ohne die vorherige ausdrückliche schriftliche Zustimmung von SPX Cooling kopiert, reproduziert, erneut veröffentlicht, hochgeladen, gepostet, öffentlich angezeigt, kodiert, übersetzt, übertragen oder in irgendeiner Weise an einen anderen Computer, Server, eine Website oder ein anderes Medium zur Veröffentlichung oder Verteilung oder für gewerbliche Unternehmen verteilt werden.

Sie dürfen die von SPX Cooling absichtlich zum Herunterladen bereitgestellten Informationen verwenden, vorausgesetzt, dass Sie (1) in allen Kopien dieser Dokumente keine Eigentumshinweise entfernen, (2) diese Informationen nur für Ihre internen Geschäftszweck verwenden und (3) keine zusätzlichen Zusicherungen oder Gewährleistungen in Bezug auf diese Informationen abgeben.

Diese Vereinbarung und alle Streitigkeiten, die sich aus oder im Zusammenhang mit dieser Vereinbarung ergeben, unterliegen den Gesetzen des US-Bundesstaates Kansas, ohne Bezugnahme auf Kollisionsnormen.

Die Produkte von SPX Cooling unterliegen ständigen Verbesserungen. SPX Cooling behält sich das Recht vor, Produktdesign, Spezifikationen und Daten ohne Vorankündigung und ohne Verpflichtung zu ändern.

de_DE