Recycled Material
Marley NC cooling towers, for example, are composed of about 70 percent recycled material when the structure is manufactured out of stainless steel or 29 percent when manufactured out of galvanized steel.
Our cooling towers frequently use gearboxes containing oil for lubrication and cooling. The Marley System 5 Geareducer has been designed to operate five years between oil changes which greatly reduces the amount of oil that needs to be recycled.
LEED Credits
It is important to note that LEED, the US national standard for green buildings, does not include large mechanical equipment such as elevators and air-conditioning equipment, which includes cooling towers, as a part of the recycled or regional sourced materials calculations.
Downloads:
Das in Großbritannien ansässige Magazin ACR News hat unseren Frage-und-Antwort-Artikel veröffentlicht, in dem Ingenieure und Designexperten befragt werden und in dem erklärt wird, wie Kühltürme zu erfolgreichen LEED-Projekten und anderen Nachhaltigkeitsinitiativen beitragen können.