Le nostre iniziative ecologiche
Office Buildings
The SPX Cooling Technologies “green” world headquarters building utilizes an evaporative cooling system. A building of its size would typically use air-cooled rooftop equipment that requires much more energy. The building was designed with numerous “healthy” building features, including effective filtration systems, and well-insulated walls and glazing for energy efficiency. Its full-perimeter windows with UV inhibition also reduce lighting energy requirements. Our company has maintained systems to recycle paper and other waste for many years.
Our three-acre underground and seven-acre aboveground Research and Development Center is heavily engaged in research to improve energy efficiency and to reduce noise, visible water vapor plume and other potential environmental impacts from cooling systems.
Marley® Cielo sereno® Plume Abatement Technology
Certain environmental conditions will introduce plume, which can lead to visibility and safety issues affecting transportation, and impact public perception. SPX overcomes these challenges through its unique ClearSky Plume Abatement technology.
ClearSky is a fully integrated system of PVC heat exchanger components that reduces the majority of water vapor before it departs the tower, eradicating common misperceptions about plume’s effect on the environment and conserving water by up to 30 percent of standard usage per year. Compared to traditional coil systems, towers equipped with ClearSky also decrease investment, maintenance and operation costs through minimized auxiliary power usage. For example, a large cooling tower fan cell can save more than 1 million gallons of water annually. Learn more about ClearSky Plume Abatement.
Removing Volatile Compounds
Manufacturing of glued thermoformed PVC film-fill has been converted to a glue system without the use of volatile organic compounds (VOCs).
Thermoformed PVC film-fill used in our crossflow HVAC cooling towers utilize a non-glued design, completely avoiding VOCs.
Download:
La rivista britannica ACR News ha pubblicato il nostro articolo di domande e risposte, intervistando ingegneri ed esperti di progettazione, che spiega come le torri di raffreddamento possono contribuire al successo dei progetti LEED e ad altre iniziative di sostenibilità.