Trusted for over 90 years.
Built on a legacy of innovation, engineered for decades of dependable performance.
The Recold® business was formed in 1932 by a team of engineers who were innovators in the fledgling refrigeration industry. Through their efforts, Recold became a technology leader and developed the first 100-ton evaporative condenser. Over 90 years later, the Recold brand continues to live up to its reputation for product value and innovation by combining solid workmanship and quality components, including copper heat exchange coil in the production of evaporative fluid coolers and condensers, as well as low-profile fluid coolers for industrial applications. The results are products that provide reliable performance, extended service life and exceptional long-term value.
Meet the Recold Team
Jon Walker
Manager of Commercial Sales –
Refrigerazione
Jon Walker
Manager of Commercial Sales - Refrigeration
Jon's bio placeholder: Jon has been with Recold since 2005. He has completed the AZ Ironman twice. This is more information about Jon. Get updated bio from him.
Rob Ochs
Refrigeration Sales
Manager
Rob Ochs
Refrigeration Sales Manager
Rob's bio placeholder: This is more information about Rob. Get updated bio from him.
Jeff Rowan
Inside Sales
Support
Jeff Rowan
Inside Sales Support
Jeff's bio placeholder: This is more information about Jeff. Get updated bio from him.
Paul Connolly
Refrigeration Product
Manager
Paul Connolly
Refrigeration Product Manager
Paul's bio placeholder: This is more information about Paul. Get updated bio from him.
Prodotti Recold
Recold is a leading manufacturer of cooling towers, fluid coolers, evaporative condensers and adiabatic cooling systems. Learn more about our Recold product line here:
RECOLD OLYMPUSV® ADIABATIC COOLING SYSTEM
RECOLD OLYMPUSV® ADIABATIC COOLING SYSTEM
IL Richiama OlympusV® Serie adiabatica equilibra il vantaggi in termini di risparmio idrico di un sistema di smaltimento del calore raffreddato ad aria con il efficienza energetica of a water-cooled solution to provide flexible cooling for operators and engineers of commercial or industrial refrigeration systems.
RECOLD JW FLUID COOLER
RECOLD JW FLUID COOLER
Il Recold JW è un rumore basso, tiraggio forzato, ventilatore centrifugo con a Bobina in rame resistente alla corrosione e a risparmio di peso in a low height configuration.
RECOLD MW FLUID COOLER
RECOLD MW FLUID COOLER
Il Recold MW è un ventilatore assiale a tiraggio indotto con a Bobina in rame resistente alla corrosione e a risparmio di peso in a low height configuration. This Evaporative Fluid Cooler is a ruggedly built unit constructed to provide many years of durable, dependable service with minimal maintenance requirements.
RECOLD MC EVAPORATIVE CONDENSER
RECOLD MC EVAPORATIVE CONDENSER
Il Recold MC è un ventilatore assiale a tiraggio indotto con a Bobina in rame resistente alla corrosione e a risparmio di peso in a configurazione ad altezza ridotta.
RECOLD LC EVAPORATIVE CONDENSER
RECOLD LC EVAPORATIVE CONDENSER
Il condensatore evaporativo Recold LC è un condensatore evaporativo in controcorrente a tiraggio indotto con tecnologia di trasferimento del calore in attesa di brevetto.
RECOLD JC EVAPORATIVE CONDENSER
RECOLD JC EVAPORATIVE CONDENSER
Il Recold JC è un progettazione a bassa rumorosità, tiraggio forzato, ventola centrifuga con un Bobina in rame resistente alla corrosione e a risparmio di peso in a altezza bassa configurazione.
RECOLD JT COOLING TOWER
RECOLD JT COOLING TOWER
La Recold JT è una torre di raffreddamento a basso profilo e a tiraggio forzato ideale per installazioni con altezza limitata. Combined with its centrifugal, ‘blower’ style fan, it is the perfetta vestibilità interna dove i soffitti sono bassi, è necessaria la canalizzazione e il rumore è inaccettabile.
Componenti aftermarket ricondizionati
Lo sono i componenti del raffreddatore di fluido, del condensatore evaporativo e della torre di raffreddamento progettati da Recold affidabile E progettato per ottimizzare le prestazioni totali del sistema e aiuto prolungare la vita del prodotto. Sappiamo che le parti di ricambio vanno ben oltre il semplice costo di acquisizione iniziale. Quando si considerano prestazioni, certificazione, affidabilità e convenienza, Recold ha senso a lungo termine. Contattaci oggi per ulteriori informazioni sulle parti aftermarket Recold
Ugelli e sistema di distribuzione Hydrospray™
XCEL® Eliminatori di deriva
Bobine di rame
Porte di accesso
Vedi anche:
Prodotti a spirale in rame da SPX Cooling Technologies e altro ancora:
Contact Our Team
Scopri di più su come i prodotti Recold supportano sistemi di refrigerazione e raffreddamento efficienti. Contattaci direttamente con questo modulo e un rappresentante Recold ti contatterà.
Telefono: 714-529-6080