Global populations are dependent on cooling and refrigeration to support many types of manufacturing and energy production processes. Evaporative cooling has been a transformative technology, enabling innovative mass production, and is substantially more energy efficient than alternatives. What may not be obvious is that evaporative cooling may also be the most water efficient option in some applications. Air conditioning is the third-largest category of commercial building energy use, after refrigeration and ventilation. Of the available methods, evaporative cooling requires the lowest energy input per unit cooling output, effectively minimizing fossil fuel usage, CO2 production and related environmental impacts. This article examines the environmental, energy and water resource realities of providing modern cooling needs and discusses resource utilization.
Noticias recientes
- SPX Cooling Introduces OlympusV™, a New Adiabatic Cooling Series of Products
- SPX Cooling anuncia la apertura de una nueva planta de fabricación de Marley® en Springfield, Missouri
- Cómo conservar agua en torres de enfriamiento evaporativo
- SPX Technologies anuncia la adquisición de TAMCO
- SPX Cooling presenta el sistema optimizador de ahorro de agua Marley® WaterGard™
- Los primeros 100 años de Marley® en los libros, el próximo siglo comienza con fuerza
- Una revisión de la eficiencia y el valor ambiental del enfriamiento evaporativo
- SPX Cooling presenta a Sean McClenaghan como presidente de refrigeración global
- SPX Cooling presenta un panel de control intuitivo con pantalla táctil HMI y modos de funcionamiento eficientes
- Las 3 principales ventajas de las bobinas de cobre en su solución de refrigeración de circuito cerrado