Cooling Tower Video Library
Présentation du système adiabatique OlympusV™
The Marley® and Recold® Adiabatic Series balances the water-saving benefits of an air-cooled heat rejection system with the energy efficiency of a water-cooled solution
Filtre pour tour de refroidissement Marley® WaterGard™
WaterGard physically blocks and rejects minerals commonly found in municipal water streams (chlorides, calcium carbonate, silica, etc.), reducing makeup water mineral content and enabling higher operating COC, resulting in reduced volume requirements for both blowdown and supply water.
Refroidissement SPX – Naturel de l’intérieur vers l’extérieur
From the outside looking in, this is just a building. A collection of walls, windows and doors. But from the inside, this is a window of opportunity.
Une école avant-gardiste installe des refroidisseurs de fluide LW
In 2015, Trevor Day School completed a new state-of-the-art vertical campus building in Manhattan’s Upper East Side. The project earned LEED Gold certification and won a 2016 AIA WHV High Honor Award. Part of the building’s sustainability initiatives was the school’s HVAC system. The building would be heated and cooled with a closed-loop “energy pile” geothermal system, one of the first systems of its kind in the U.S. When the system needed to expand its heating/cooling abilities in 2022, the project engineers turned to SPX Cooling Tech for a solution. The team chose to install induced-draft, closed-circuit Marley LW Fluid Coolers for more efficient heat rejection. Marley LW fluid coolers are designed to be installed quickly and offer a small footprint for easier integration into existing systems. These towers are delivered with factory-installed controls, factory wired and tested and are equipped with ultra-efficient, corrosion-resistant copper coils. To reduce the heat of their process fluids, the school would need two LW units. The units were hoisted into position using a crane that reached 200+ ft. into the air to install the fluid coolers onto a newly created platform atop the school’s roof. Installation was completed in a single day and the systems were ready to go just before the beginning of the school year. For more about the LW, and other closed-circuit cooling tower solutions, visit spxcooling.com/fluidcoolers.
Présentation de SPX Corporation
SPX Corporation is, along with its subsidiaries, a diversified, global supplier of infrastructure equipment with scalable growth platforms in heating, ventilation and air conditioning (HVAC), and detection and measurement. With operations in 15 countries and more than $1 billion in annual revenue, we offer a wide array of highly engineered products with strong brands.
Sélections d'un siècle de Marley
Une brève histoire de la marque Marley et des produits Marley tout au long de nos 100 ans d'histoire.
Installation du filtre Marley® BasinGard™ pour les tours NC8400
Le filtre Marley BasinGard permet d'économiser du temps et de l'argent en simplifiant le nettoyage du bassin d'eau chaude d'une tour de refroidissement et en protégeant les composants de la tour de refroidissement.
Présentation du sélecteur de produits de tour de refroidissement CoolSpec™
CoolSpec™ Selection Software is a new, intuitive tool that compares and selects Marley® and Recold® brand evaporative cooling products - open-circuit and closed-circuit, crossflow and counterflow - cooling towers, fluid coolers and evaporative condensers.
Tours de refroidissement par évaporation dans le processus du centre de données
La puissance de calcul massive des centres de données génère de la chaleur, ce qui fait d’un refroidissement efficace une exigence clé du système du bâtiment. Les tours de refroidissement par évaporation font partie intégrante de nombreux systèmes de refroidissement de centres de données.
Installation du filtre Marley® BasinGard™ pour les tours NC8300
Le filtre Marley BasinGard permet d'économiser du temps et de l'argent en simplifiant le nettoyage du bassin d'eau chaude d'une tour de refroidissement et en protégeant les composants de la tour de refroidissement.
Teaser de la tour de refroidissement modulaire Marley®
SPX Cooling Technologies’ innovative modular cooling tower construction concepts support safety initiatives, compressed schedules, fewer working hands on-site and more. Contact your local sales representative to watch the full video and learn more about modular cooling tower options: /rep-search/
Présentation du refroidisseur de fluide Marley MH Element™
La gamme populaire de refroidisseurs de fluide Marley MH s'est élargie pour inclure des modèles supplémentaires. Le refroidisseur de fluide Marley MH Element™, associé à l'ajout de serpentins en cuivre, offre la plus grande efficacité par empreinte au sol.
Présentation du condenseur évaporatif industriel SGS
Répondant à votre besoin d'un condenseur évaporatif industriel de qualité, comptez sur le nouveau condenseur évaporatif industriel SGS qui sera conçu avec précision et fabriqué avec soin.
Installation de la tour de refroidissement Marley NC Everest – Hôpital Adan
One of the largest hospitals in Kuwait designed its cooling system with 6 cells of the Marley NC Everest Cooling Tower. With up to 50% greater cooling capacity, the tower cells serve five 1,850-ton chillers and offer higher energy savings, fewer components and lower maintenance costs!
Comment installer une tour de refroidissement Marley® NC® Épisode 13 : Cylindre de ventilateur
Les cylindres de ventilateur Marley® sont des composants essentiels pour protéger les pales du ventilateur, minimiser le bruit et les vibrations et faciliter des performances optimales dans toutes les applications de tour de refroidissement.
Logiciel de sélection de tour de refroidissement Marley FIT
Our new Marley FIT air delivery selection software takes into consideration the relationship among all cooling tower mechanical system components to recommend a complete system. Air flow is directly proportional to the thermal performance of your cooling tower. Using performance data derived from the SPX Research and Development Center and independently tested and verified, Marley FIT Selection Software facilitates maximum cooling tower performance and maximum value. Get FIT. Register now at www.marleyfit.com.
Comment installer une tour de refroidissement Marley® NC® Épisode 12 : Canaux et vannes de déversoir
Sur les tours de refroidissement NC comportant plus d'une cellule, un ensemble de canaux d'interconnexion pour égaliser et maintenir un niveau d'eau approprié entre plusieurs bassins de collecte est une option.
Comment installer une tour de refroidissement Marley® NC® Épisode 11 : Moteur à l'extérieur du flux d'air
Sur les tours équipées d'une option Motor Outside Airstream ou MOA, le moteur, le support moteur et l'arbre de transmission sont installés et alignés sur site.
Comment installer une tour de refroidissement Marley® NC® Épisode 10 : Assemblage et installation de l'échelle
Si votre tour de refroidissement Marley NC comprend une échelle en option pour accéder au ventilateur, regardez cette vidéo pour garantir une installation et une configuration correctes.
Comment installer une tour de refroidissement Marley® NC® Épisode 9 : Garde-corps pour échelle frontale d'entrée d'air
Si votre tour de refroidissement Marley NC comprend un garde-corps en option pour une échelle frontale d'entrée d'air (persienne), regardez cette vidéo pour garantir une installation et une configuration correctes.
Comment installer une tour de refroidissement Marley® NC® Épisode 8 : Garde-corps pour échelle à façade gainée
Si votre tour de refroidissement Marley NC comprend un garde-corps en option pour une échelle frontale à caisson, regardez cette vidéo pour garantir une installation et une configuration correctes.
Marley Cooling Tower Advanced Basin Heater (ABH)
The Marley ABH (Advanced Basin Heater) Control Panel controls on/off operation of the cold water basin heater(s) and prevents freezing in cold environments. Watch a Marley Expert discuss the features, benefits and operation of the Marley Advanced Basin Heater cooling tower control panel.
Comment installer une tour de refroidissement Marley® NC® Épisode 7 : Vannes HC
Si votre tour de refroidissement Marley NC comprend des vannes de commande horizontale (HC) en option, regardez cette vidéo pour garantir une installation et une configuration correctes.
Comment installer une tour de refroidissement Marley® NC® Épisode 6 : Protections de ventilateur
Suivez ces directives pour accélérer le processus et garantir le placement correct de la protection du ventilateur sur votre tour de refroidissement Marley NC.
Comment installer une tour de refroidissement Marley® NC® Épisode 5 : Trucs et astuces modulaires
Afin d'assembler et d'installer correctement les tours de refroidissement NC modulaires, suivez ces directives pour éviter les erreurs courantes et accélérer le processus d'installation de la tour de refroidissement.
Comment installer une tour de refroidissement Marley® NC® Épisode 4 : Modules de levage
Suivez ces directives de levage simples et l'ensemble du processus de levage de votre tour de refroidissement Marley NC sera fluide et efficace.
Comment installer une tour de refroidissement Marley® NC® Épisode 3 : Matériel nécessaire
Afin d'assembler et d'installer correctement une tour de refroidissement Marley NC, votre équipe devra être préparée avec quelques outils de base, et vous devrez également connaître certains équipements et procédures de base.
Comment installer une tour de refroidissement Marley® NC® Épisode 2 : Instructions d'installation et dessins
Le pack de documentation Marley NC comprend vos instructions d'installation, votre nomenclature et vos dessins d'installation pour tous les composants standard et optionnels de la tour de refroidissement NC.
Comment installer une tour de refroidissement Marley NC Épisode 1 : Préparation du site, arrivée de la tour et déchargement
Suivez ces directives simples et l'ensemble du processus d'arrivée et de déchargement de votre tour de refroidissement NC sera fluide et efficace.
Marley Cooling Tower Fan Test Facility
For over two decades, every Marley cooling tower fan has been accurately verified for field performance in this model fan test cell. Get an inside look here:
Refroidisseur de fluide Marley DT
Take a look at the Marley DT Fluid Cooler, now with a new finned coil option for expanded dry capacity and thermal performance!
Série de tours de refroidissement Marley® NC® – Comparaison taille/capacité
Just how big is a Marley NC Everest cooling tower compared to other Marley NC cooling tower models? Take a look at the differences between Marley NC8407, the Marley NC8414 and the Marley NC8422 cooling towers!
Flux croisé contre. Tours de refroidissement à contre-courant
Quelle est la différence entre une tour de refroidissement à flux croisé et à contre-courant ? SPX Cooling Tech démontre les différences et les avantages de chaque conception.
Ensemble de tour de refroidissement Marley® NC Everest®
Regardez la toute première tour de refroidissement Marley® NC Everest® être assemblée au centre de recherche et de développement SPX.
Vannes de régulation de débit pour tour de refroidissement Marley® HC
Les vannes Marley® HC offrent une faible vitesse de décharge et confinent les éclaboussures, ce qui entraîne une faible chute de pression. Apprenez-en davantage sur leur impact sur les performances de votre tour de refroidissement ici :
Marley® Quadraflow Maintenance
The QuadraFlow’s unique, compact design is matched by its performance, maintainability, and reliability. Watch a Marley expert discuss the advantages and proper maintenance of the Marley Quadraflow cooling tower.
Didcot B Power Station Cooling Tower Repair
Follow our Time Lapse video as SPX repairs Didcot B Power Station's cooling tower cells to their original design following an unfortunate fire that severely damaged more than three cells.
Le remplissage de ma tour de refroidissement est-il sale ?
How do you know when it is time to replace your cooling tower fill? Watch a Marley expert discuss how to tell the difference cooling tower fill with normal scale build-up and clogged fill that needs maintenance.
Marley® Cooling Tower Integral Louvers
What are integral louvers, and what difference do they make in the operation, cost and performance of your cooling tower? Watch as we discuss the advantages.
301L vs 304 Stainless Steel
The type of steel used in the construction of your cooling tower makes a difference. In this video, we'll discuss the advantages of using 301L stainless steel in your Marley cooling tower.
Marley® Geareducer® Cooling Tower Gearbox Oil Change
How do I change my cooling tower's gearbox oil? The process of changing the oil in your Marley Geareducer cooling tower gearbox is straightforward - watch a Marley expert demonstrate in this video.
Cooling Tower Gear Drives Vs. Belt Drives
Some cooling towers power their fans with belt drives, and some use gear drives. But which is better for your application? In this video, we discuss the benefits of using a Marley Geareducer gear drive over a belt drive in your cooling tower.
Marley NCWD Cooling Tower Lift
The NCWD is an innovative, patented factory assembled hybrid cooling tower designed specifically for plume reduction. Watch as this NCWD is lifted in London, England.
Marley MBX EZ Pack Cooling Tower Fill
The MBX EZ Pack fill's contractor-friendly fill design makes installation fast and easy without requiring major tower modifications.
Marley MD Everest Cooling Tower Assembly
The MD Everest Cooling Tower is uniquely suited for applications with higher cooling demands, including data centers, district energy complexes, health science campuses and industrial complexes. Watch as a new Marley MD Everest modular cooling tower is assembled in this video.
Installation du Geareducer® Marley® série M
Lorsque les boîtes de vitesses de ce client ont commencé à subir des vibrations et des dommages aux engrenages, ils ont fait appel à Marley pour obtenir des renforts. Regardez avec quelle facilité les anciennes boîtes de vitesses ont été remplacées par des entraînements à engrenages Marley dans cette vidéo.
Écrans d'entrée d'air pour tour de refroidissement Marley®
Si votre tour de refroidissement présente une accumulation de débris ou un colmatage, les grilles d'entrée d'air Marley sont une solution. Regardez nous discuter des avantages de l’utilisation de grilles d’entrée d’air sur votre tour de refroidissement.
Marley Parts Vodcast 1 of 3: Geareducer
Jerome Jennings from Marley / SPX Cooling Tech. explains the benefits of using a genuine Marley Geareducer gearbox (Marley Parts Vodcast Part 1 of 3).
Marley Parts Vodcast 2 of 3: Driveshafts
Jerome Jennings from Marley / SPX Cooling Technologies explains the benefits of using a genuine Marley driveshaft (Marley Parts Vodcast Part 2 of 3).
Marley Parts Vodcast 3 of 3: Fan Blades
Jerome Jennings from Marley / SPX Cooling Technologies explains the benefits of using genuine Marley Fan Blades (Marley Parts Vodcast Part 3 of 3).
Marley Cooling Tower Bearing Lubrication
It's important to properly maintain your Marley cooling tower bearings. Watch as a Marley expert provides some helpful tips for making bearing lubrication easy.
Marley NS Cooling Tower Spray System Overview
Marley NS counterflow nozzles develop uniform water distribution over a wide range of operating water pressures, and NS counterflow nozzles have no internal parts or narrow passageways to get clogged with debris.
Marley Geareducer Rebuild and Repair
Whether you have questions on Marley Geareducer cooling tower gearbox operation and maintenance, need components to perform a repair yourself, or want to send your unit back to us for the highest level of care, SPX has the solution.
Système de buse et de coupelle Marley ST
The Marley Spiral Target nozzle and cup system is an injection molded polypropylene unit consisting of two parts — the main body with integral target diffuser and a snap-on insert or orifice cap. Watch here to learn more.
Refroidisseur de fluide Marley MH
The popular Marley MH Fluid Cooler line has expanded to include additional models, all capable of incorporating copper coils for increased thermal capacity. Watch a quick product overview here.
Marley Cooling Tower Mechanical Float System
What are the advantages to a Marley mechanical cooling tower float system? Why would your cooling tower benefit from a float system? Learn more by watching.
Marley MD Cooling Tower Overview
The Marley MD is a factory-assembled, counterflow cooling tower. For many HVAC and light industrial applications, this design requires less plan area and offers greater site placement flexibility than a comparable crossflow cooling tower.
Marley Geareducer® Gearbox Overview
The reliability of the Geareducer comes from more than 100,000 units of experience, and from Marley’s attention to exacting quality standards of design and manufacturing. Today, every Marley Geareducer is tested under load at our factory. Then, it’s inspected and adjusted before shipment.
Marley Cooling Tower Maintenance
Diagnosing maintenance issues often begins with inspection of mechanical equipment and components subject to wear and tear – for example, motors, gearboxes or belt drives.
Marley Cooling Tower Duty Motor
Cooling tower duty motors in Marley products are built according to NEMA standards and designed to withstand exposure to hot, moist cooling tower conditions. Additionally, to support long service life, the motor’s interior is fan-cooled and coated with epoxy for maximum protection from heat, moisture and corrosion.
Marley Cooling Tower HC Flow Control Valve
HC valve body proportions and the arrangement of internal parts provide a low discharge velocity and confine splash, resulting in low pressure drop. Watch to learn more about HC valve operation.
Ultra Quiet Fan Blade Pitch Adjustment
The Ultra Quiet fan is designed for HVAC cooling tower applications where very low sound is a necessity. Here's a demonstration on how to adjust the blade pitch on your cooling tower's Ultra Quiet Fan.
Marley X7 Blade Pitch Adjustment
The Marley X7 fan is designed for induced-draft cooling tower applications, offering distinct advantages over other fan designs. Watch this video to learn how to adjust your cooling tower's X7 fan blades.
Marley H3 Cooling Tower Fan Blade Pitch Adjustment
How do you adjust the blade pitch on your Marley H3 fan blades? Marley engineers demonstrate the process, including what tools are needed to complete the job.
Marley Cooling Tower Belt Drive Components
In this video, learn about Marley belt drive components and view a demonstration of belt tensioning and sheave alignment for your cooling tower's belt drive system.
Marley Cooling Tower Hanging Fill Replacement
What's the best way to replace the hanging fill in your cooling tower? Watch a demonstration of quick and easy Marley cooling tower fill replacement here.
Marley MBX Cooling Tower Fill Packs
Robert Swafford from Marley demonstrates the right way to quickly and easily replace your cooling tower's dirty fill with Marley MBX fill packs.
Proof in Performance – Heat Transfer Fill Part 3
What are the benefits of using genuine Marley heat transfer fill? Learn all about it from a Marley expert: (Part 3 of 3).
Proof in Performance – Heat Transfer Fill Part 2
What are the benefits of using genuine Marley heat transfer fill? Learn all about it from a Marley expert: (Part 2 of 3).
Proof In Performance – Heat Transfer Fill Part 1
What are the benefits of using genuine Marley heat transfer fill? Learn all about it from a Marley expert: (Part 1 of 3).
Marley NC Entrée inférieure unique
Quels sont les avantages de l'entrée inférieure unique dans une tour de refroidissement Marley NC et comment joue-t-elle un rôle dans l'efficacité et la maintenance de la tour de refroidissement ?
Marley Cooling Tower Drive Shaft Alignment
Couplings and driveshafts must be strong, durable, and aligned properly to efficiently transmit power from the cooling tower motor to the gearbox. Watch a demonstration of how to use the Marley Dial Indicator Kit to align a Marley cooling tower driveshaft here:
Ajustement du couplage de la série Marley MC
If your cooling tower utilizes a Marley MC series coupling, it might need to be occasionally maintained or adjusted. Watch here as we demonstrate how to perform basic maintenance and adjustments on a typical Marley MC series coupling.
Marley Pinion Shaft Oil Seal Replacement
Marley cooling tower gearboxes are equipped with long-life pinion oil seals. If the pinion shaft oil seal on your cooling tower's gearbox has become worn or is leaking, watch here as we demonstrate the best way to replace it.
Commutateur de vibration mécanique Marley
Cooling tower vibration switches trigger an alarm and/or shut down equipment when excessive vibration occurs. Watch here as a Marley product expert demonstrates the functionality of a mechanical vibration switch, including how to test that functionality in the field.
Marley LLC Water Level Control Part 9 – Troubleshooting The Connection Points
Marley LLC Water Level Control systems monitor and adjust the water level in the cooling tower cold water collection basin. Watch our Marley Controls expert as he provides an overview of LLC operation (part 9 of 9: Troubleshooting the Connection Points).
Marley LLC Water Level Control Part 8 – Troubleshooting The Solenoid Valve
Marley LLC Water Level Control systems monitor and adjust the water level in the cooling tower cold water collection basin. Watch our Marley Controls expert as he provides an overview of LLC operation (part 8 of 9: Troubleshooting the Solenoid Valve).
Marley LLC Water Level Control Part 7 – Troubleshooting The Makeup Card
Marley LLC Water Level Control systems monitor and adjust the water level in the cooling tower cold water collection basin. Watch our Marley Controls expert as he provides an overview of LLC operation (part 7 of 9: Testing the Makeup Card).
Marley LLC Water Level Control Part 6 – Troubleshooting The Panel
Marley LLC Water Level Control systems monitor and adjust the water level in the cooling tower cold water collection basin. Watch our Marley Controls expert as he provides an overview of LLC operation (part 6 of 9: Troubleshooting).
Marley LLC Water Level Control Part 5 – Testing
Marley LLC Water Level Control systems monitor and adjust the water level in the cooling tower cold water collection basin. Watch our Marley Controls expert as he provides an overview of LLC operation (part 5 of 9: Control Panel).
Marley LLC Water Level Control Part 4 – Control Panel
Marley LLC Water Level Control systems monitor and adjust the water level in the cooling tower cold water collection basin. Watch our Marley Controls expert as he provides an overview of LLC operation (part 4 of 9: Control Panel).
Marley LLC Water Level Control Part 3 – Start Up
Marley LLC Water Level Control systems monitor and adjust the water level in the cooling tower cold water collection basin. Watch our Marley Controls expert as he provides an overview of LLC operation (part 3 of 9: Start-Up).
Marley LLC Water Level Control Part 2 – Installation
Marley LLC Water Level Control systems monitor and adjust the water level in the cooling tower cold water collection basin. Watch our Marley Controls expert as he provides an overview of LLC operation (part 2 of 9: Installation).
Marley LLC Water Level Control Part 1 – Introduction
Marley LLC Water Level Control systems monitor and adjust the water level in the cooling tower cold water collection basin. Watch our Marley Controls expert as he provides an overview of LLC operation (part 1 of 9: Introduction).
Marley Cooling Tower Drift Eliminator
Low drift rates are the primary goal of a drift eliminator. Marley drift eliminator advancements can yield drift rates as low as 0.0005% of design flow rates. This video reviews the advantages of using Marley's newly redesigned drift eliminators.
Marley NC Internal Accessibility
The Marley NC cooling tower's two large access doors provide non-confining, quick visual inspection of cold water basin, internal structure, drift eliminators and mechanical equipment in the plenum area. Take a look:
Expanded Geareducer Cooling Tower Gearbox Line
Marley Series M Geareducers are designed and manufactured to directly replace other OEM gearboxes in cooling towers for power and industrial applications.
NC Everest Cooling Tower Walkthrough
SPX Cooling Technologies embarked on a mission to design and build a cooling tower like no other in the world. Like adventurers climbing Mt. Everest, we knew the challenges yet were driven to achieve something remarkable. Watch here.
Marley NC Everest Aperçu
Soyez enthousiasmé par la toute nouvelle tour de refroidissement Marley NC Everest !
Marley Cooling Tower Gearbox Repair Program
Whether you have questions on Geareducer operation and maintenance, need components to perform a repair yourself, or want to send your unit back to us for the highest level of care, SPX has the solution.
Cube Installation
In this video, learn more about the SGS Cube evaporative condenser assembly and installation process.
Réduction du panache de la tour de refroidissement Marley ClearSky
Il existe de nombreuses raisons pour lesquelles vous souhaiterez peut-être réduire le panache visible de votre tour de refroidissement. La réduction du panache Marley ClearSky est un système entièrement intégré qui fonctionne de manière plus fiable que les systèmes à serpentins.
Ascenseur de tour de refroidissement
Regardez une tour de refroidissement Marley NC être transportée dans un hôpital d'Overland Park, au Kansas.
Installation de la tour de refroidissement TDI NC
Regardez TDI installer des tours de refroidissement Marley NC sur la tour de Thanksgiving à Dallas, au Texas.
Marley Modular F400 Cooling Tower
SPX Cooling Tech’s innovative modular cooling tower construction concepts support safety initiatives, compressed schedules, fewer working hands on-site and more. Watch a showcase of the new Marley Modular F400 Cooling Tower here:
Marley NC Cooling Tower Overview
The Marley NC Cooling Tower has set the standard for high efficiency and low maintenance since its introduction in 1968. Learn more about cooling tower performance by watching an overview of the Marley NC cooling tower here: