Cooling Tower Video Library
Introducing the OlympusV™ Adiabatic System
The Marley® and Recold® Adiabatic Series balances the water-saving benefits of an air-cooled heat rejection system with the energy efficiency of a water-cooled solution
Filtro per torre di raffreddamento Marley® WaterGard™
WaterGard physically blocks and rejects minerals commonly found in municipal water streams (chlorides, calcium carbonate, silica, etc.), reducing makeup water mineral content and enabling higher operating COC, resulting in reduced volume requirements for both blowdown and supply water.
Raffreddamento SPX: naturale dall'interno
From the outside looking in, this is just a building. A collection of walls, windows and doors. But from the inside, this is a window of opportunity.
Una scuola lungimirante installa i raffreddatori di fluido LW
In 2015, Trevor Day School completed a new state-of-the-art vertical campus building in Manhattan’s Upper East Side. The project earned LEED Gold certification and won a 2016 AIA WHV High Honor Award. Part of the building’s sustainability initiatives was the school’s HVAC system. The building would be heated and cooled with a closed-loop “energy pile” geothermal system, one of the first systems of its kind in the U.S. When the system needed to expand its heating/cooling abilities in 2022, the project engineers turned to SPX Cooling Tech for a solution. The team chose to install induced-draft, closed-circuit Marley LW Fluid Coolers for more efficient heat rejection. Marley LW fluid coolers are designed to be installed quickly and offer a small footprint for easier integration into existing systems. These towers are delivered with factory-installed controls, factory wired and tested and are equipped with ultra-efficient, corrosion-resistant copper coils. To reduce the heat of their process fluids, the school would need two LW units. The units were hoisted into position using a crane that reached 200+ ft. into the air to install the fluid coolers onto a newly created platform atop the school’s roof. Installation was completed in a single day and the systems were ready to go just before the beginning of the school year. For more about the LW, and other closed-circuit cooling tower solutions, visit spxcooling.com/fluidcoolers.
Panoramica della SPX Corporation
SPX Corporation is, along with its subsidiaries, a diversified, global supplier of infrastructure equipment with scalable growth platforms in heating, ventilation and air conditioning (HVAC), and detection and measurement. With operations in 15 countries and more than $1 billion in annual revenue, we offer a wide array of highly engineered products with strong brands.
Selezioni da un secolo di Marley
Una breve storia del marchio Marley e dei prodotti Marley attraverso i nostri 100 anni di storia.
Installazione del filtro Marley® BasinGard™ per torri NC8400
Il filtro Marley BasinGard consente di risparmiare tempo e denaro semplificando la pulizia del bacino dell'acqua calda di una torre di raffreddamento e proteggendo i componenti della torre di raffreddamento.
Presentazione del selettore di prodotti per torri di raffreddamento CoolSpec™
CoolSpec™ Selection Software is a new, intuitive tool that compares and selects Marley® and Recold® brand evaporative cooling products - open-circuit and closed-circuit, crossflow and counterflow - cooling towers, fluid coolers and evaporative condensers.
Torri di raffreddamento evaporative nel processo del Data Center
L'enorme potenza di calcolo dei data center genera calore, rendendo il raffreddamento efficiente un requisito fondamentale del sistema edilizio. Le torri di raffreddamento evaporative sono parte integrante di molti sistemi di raffreddamento dei data center.
Installazione del filtro Marley® BasinGard™ per torri NC8300
Il filtro Marley BasinGard consente di risparmiare tempo e denaro semplificando la pulizia del bacino dell'acqua calda di una torre di raffreddamento e proteggendo i componenti della torre di raffreddamento.
Teaser della torre di raffreddamento modulare Marley®
SPX Cooling Technologies’ innovative modular cooling tower construction concepts support safety initiatives, compressed schedules, fewer working hands on-site and more. Contact your local sales representative to watch the full video and learn more about modular cooling tower options: /rep-search/
Presentazione del raffreddatore di fluidi Marley MH Element™
La popolare linea di raffreddatori a fluido Marley MH si è ampliata per includere modelli aggiuntivi. Il raffreddatore di fluido Marley MH Element™ con l'aggiunta di serpentine in rame offre la massima efficienza in termini di ingombro.
Presentazione del condensatore evaporativo industriale SGS
Rispondendo alla vostra esigenza di un condensatore evaporativo industriale di qualità, potete contare sul nuovo condensatore evaporativo industriale SGS progettato con precisione e prodotto con cura.
Installazione della torre di raffreddamento Marley NC Everest – Ospedale Adan
One of the largest hospitals in Kuwait designed its cooling system with 6 cells of the Marley NC Everest Cooling Tower. With up to 50% greater cooling capacity, the tower cells serve five 1,850-ton chillers and offer higher energy savings, fewer components and lower maintenance costs!
Come installare una torre di raffreddamento Marley® NC® Episodio 13: Cilindro della ventola
I cilindri delle ventole Marley® sono componenti cruciali per proteggere le pale delle ventole, ridurre al minimo il rumore e le vibrazioni e facilitare prestazioni ottimali in tutte le applicazioni delle torri di raffreddamento.
Software di selezione delle torri di raffreddamento Marley FIT
Our new Marley FIT air delivery selection software takes into consideration the relationship among all cooling tower mechanical system components to recommend a complete system. Air flow is directly proportional to the thermal performance of your cooling tower. Using performance data derived from the SPX Research and Development Center and independently tested and verified, Marley FIT Selection Software facilitates maximum cooling tower performance and maximum value. Get FIT. Register now at www.marleyfit.com.
Come installare una torre di raffreddamento Marley® NC® Episodio 12: Canali e chiuse
Sulle torri di raffreddamento NC con più di una cella, è opzionale un gruppo di canali di interconnessione per equalizzare e mantenere il livello adeguato dell'acqua tra più bacini di raccolta.
Come installare una torre di raffreddamento Marley® NC® Episodio 11: Motore esterno al flusso d'aria
Sulle torri con opzione Motor Outside Airstream o MOA, il motore, il supporto motore e l'albero di trasmissione vengono installati e allineati in loco.
Come installare una torre di raffreddamento Marley® NC® Episodio 10: Assemblaggio e installazione della scala
Se la tua torre di raffreddamento Marley NC include una scala opzionale per accedere al fan deck, guarda questo video per garantire la corretta installazione e configurazione.
Come installare una torre di raffreddamento Marley® NC® Episodio 9: Guardrail per scala frontale di ingresso dell'aria
Se la tua torre di raffreddamento Marley NC include un parapetto opzionale per una scala frontale di ingresso dell'aria (aletta), guarda questo video per garantire un'installazione e una configurazione corrette.
Come installare una torre di raffreddamento Marley® NC® Episodio 8: Guardrail per scala frontale rivestita
Se la tua torre di raffreddamento Marley NC include un parapetto opzionale per una scala frontale rivestita, guarda questo video per garantire la corretta installazione e configurazione.
Riscaldatore avanzato per bacino Marley Cooling Tower (ABH)
The Marley ABH (Advanced Basin Heater) Control Panel controls on/off operation of the cold water basin heater(s) and prevents freezing in cold environments. Watch a Marley Expert discuss the features, benefits and operation of the Marley Advanced Basin Heater cooling tower control panel.
How To Install A Marley® NC® Cooling Tower Episode 7: HC Valves
If your Marley NC Cooling Tower includes optional Horizontal Control (HC) Valves, watch this video to ensure proper installation and configuration.
How To Install A Marley® NC® Cooling Tower Episode 6: Fan Guards
Follow these guidelines to speed the process and ensure correct placement of the fan guard on your Marley NC Cooling Tower.
How To Install A Marley® NC® Cooling Tower Episode 5: Modular Tips and Tricks
In order to correctly assemble and install modular NC Cooling Towers, follow these guidelines to avoid common mistakes and speed the cooling tower installation process.
How To Install A Marley® NC® Cooling Tower Episode 4: Hoisting Modules
Follow these simple hoisting guidelines and the entire process for hoisting your Marley NC cooling tower into place will be smooth and efficient.
How To Install A Marley® NC® Cooling Tower Episode 3: Necessary Hardware
In order to correctly assemble and install a Marley NC Cooling Tower, your team will need to be prepared with some basic tools, and you should also be aware of some basic equipment and procedures.
How To Install A Marley® NC® Cooling Tower Episode 2: Installation Instructions and Drawings
The Marley NC literature pack includes your installation instructions, bill of materials, and installation drawings for all NC cooling tower’s standard and optional components.
How To Install A Marley NC Cooling Tower Episode 1: Site Prep, Tower Arrival and Unloading
Follow these simple guidelines and the entire process for your NC Cooling Tower’s arrival and unloading will be smooth and efficient.
Marley Cooling Tower Fan Test Facility
For over two decades, every Marley cooling tower fan has been accurately verified for field performance in this model fan test cell. Get an inside look here:
Raffreddatore di liquidi Marley DT
Take a look at the Marley DT Fluid Cooler, now with a new finned coil option for expanded dry capacity and thermal performance!
Marley® NC® Cooling Tower Series – Size/Capacity Comparison
Just how big is a Marley NC Everest cooling tower compared to other Marley NC cooling tower models? Take a look at the differences between Marley NC8407, the Marley NC8414 and the Marley NC8422 cooling towers!
Flusso incrociato vs. Torri di raffreddamento in controcorrente
Qual è la differenza tra una torre di raffreddamento a flusso incrociato e una a flusso controcorrente? SPX Cooling Tech dimostra le differenze e i vantaggi di ciascun progetto.
Marley® NC Everest® Cooling Tower Assembly
Watch as the very first Marley® NC Everest® cooling tower is assembled at the SPX Research and Development Center.
Marley® HC Cooling Tower Flow Control Valves
Marley® HC valves provide a low discharge velocity and confine splash, resulting in low pressure drop. Learn more about how they impact your cooling tower performance here:
Marley® Quadraflow Maintenance
The QuadraFlow’s unique, compact design is matched by its performance, maintainability, and reliability. Watch a Marley expert discuss the advantages and proper maintenance of the Marley Quadraflow cooling tower.
Didcot B Power Station Cooling Tower Repair
Follow our Time Lapse video as SPX repairs Didcot B Power Station's cooling tower cells to their original design following an unfortunate fire that severely damaged more than three cells.
Il riempimento della mia torre di raffreddamento è sporco?
Come fai a sapere quando è il momento di sostituire il riempimento della torre di raffreddamento? Guarda un esperto Marley discutere su come distinguere il riempimento della torre di raffreddamento da un normale accumulo di calcare e un riempimento intasato che necessita di manutenzione.
Marley® Cooling Tower Integral Louvers
What are integral louvers, and what difference do they make in the operation, cost and performance of your cooling tower? Watch as we discuss the advantages.
Acciaio inossidabile 301L rispetto a 304
Il tipo di acciaio utilizzato nella costruzione della tua torre di raffreddamento fa la differenza. In questo video discuteremo dei vantaggi derivanti dall'utilizzo dell'acciaio inossidabile 301L nella tua torre di raffreddamento Marley.
Marley® Geareducer® Cooling Tower Gearbox Oil Change
How do I change my cooling tower's gearbox oil? The process of changing the oil in your Marley Geareducer cooling tower gearbox is straightforward - watch a Marley expert demonstrate in this video.
Cooling Tower Gear Drives Vs. Belt Drives
Some cooling towers power their fans with belt drives, and some use gear drives. But which is better for your application? In this video, we discuss the benefits of using a Marley Geareducer gear drive over a belt drive in your cooling tower.
Marley NCWD Cooling Tower Lift
The NCWD is an innovative, patented factory assembled hybrid cooling tower designed specifically for plume reduction. Watch as this NCWD is lifted in London, England.
Marley MBX EZ Pack Cooling Tower Fill
The MBX EZ Pack fill's contractor-friendly fill design makes installation fast and easy without requiring major tower modifications.
Marley MD Everest Cooling Tower Assembly
The MD Everest Cooling Tower is uniquely suited for applications with higher cooling demands, including data centers, district energy complexes, health science campuses and industrial complexes. Watch as a new Marley MD Everest modular cooling tower is assembled in this video.
Marley® M Series Geareducer® Installation
When this customer's gearboxes started to experience vibration and gear damage, they called in Marley for reinforcements. Watch how easily the old gearboxes were replaced with Marley gear drives in this video.
Marley® Cooling Tower Air Inlet Screens
If your cooling tower is experiencing debris buildup or fill clogging, Marley air inlet screens are one solution. Watch as we discuss the advantages of using air inlet screens on your cooling tower.
Marley Parts Vodcast 1 of 3: Geareducer
Jerome Jennings from Marley / SPX Cooling Tech. explains the benefits of using a genuine Marley Geareducer gearbox (Marley Parts Vodcast Part 1 of 3).
Marley Parts Vodcast 2 of 3: Driveshafts
Jerome Jennings from Marley / SPX Cooling Technologies explains the benefits of using a genuine Marley driveshaft (Marley Parts Vodcast Part 2 of 3).
Marley Parts Vodcast 3 of 3: Fan Blades
Jerome Jennings from Marley / SPX Cooling Technologies explains the benefits of using genuine Marley Fan Blades (Marley Parts Vodcast Part 3 of 3).
Marley Cooling Tower Bearing Lubrication
It's important to properly maintain your Marley cooling tower bearings. Watch as a Marley expert provides some helpful tips for making bearing lubrication easy.
Marley NS Cooling Tower Spray System Overview
Marley NS counterflow nozzles develop uniform water distribution over a wide range of operating water pressures, and NS counterflow nozzles have no internal parts or narrow passageways to get clogged with debris.
Marley Geareducer Rebuild and Repair
Whether you have questions on Marley Geareducer cooling tower gearbox operation and maintenance, need components to perform a repair yourself, or want to send your unit back to us for the highest level of care, SPX has the solution.
Sistema di ugelli e tazze Marley ST
The Marley Spiral Target nozzle and cup system is an injection molded polypropylene unit consisting of two parts — the main body with integral target diffuser and a snap-on insert or orifice cap. Watch here to learn more.
Raffreddatore di liquidi Marley MH
The popular Marley MH Fluid Cooler line has expanded to include additional models, all capable of incorporating copper coils for increased thermal capacity. Watch a quick product overview here.
Marley Cooling Tower Mechanical Float System
What are the advantages to a Marley mechanical cooling tower float system? Why would your cooling tower benefit from a float system? Learn more by watching.
Panoramica della torre di raffreddamento Marley MD
La Marley MD è una torre di raffreddamento in controcorrente assemblata in fabbrica. Per molte applicazioni HVAC e dell'industria leggera, questo design richiede meno area in pianta e offre una maggiore flessibilità di posizionamento del sito rispetto a una torre di raffreddamento a flusso incrociato comparabile.
Marley Geareducer® Gearbox Overview
The reliability of the Geareducer comes from more than 100,000 units of experience, and from Marley’s attention to exacting quality standards of design and manufacturing. Today, every Marley Geareducer is tested under load at our factory. Then, it’s inspected and adjusted before shipment.
Marley Cooling Tower Maintenance
Diagnosing maintenance issues often begins with inspection of mechanical equipment and components subject to wear and tear – for example, motors, gearboxes or belt drives.
Marley Cooling Tower Duty Motor
Cooling tower duty motors in Marley products are built according to NEMA standards and designed to withstand exposure to hot, moist cooling tower conditions. Additionally, to support long service life, the motor’s interior is fan-cooled and coated with epoxy for maximum protection from heat, moisture and corrosion.
Marley Cooling Tower HC Flow Control Valve
HC valve body proportions and the arrangement of internal parts provide a low discharge velocity and confine splash, resulting in low pressure drop. Watch to learn more about HC valve operation.
Regolazione del passo delle pale della ventola ultra silenziosa
La ventola ultra silenziosa è progettata per applicazioni in torri di raffreddamento HVAC in cui è necessaria una rumorosità molto bassa. Ecco una dimostrazione su come regolare l'inclinazione delle pale della ventola ultra silenziosa della tua torre di raffreddamento.
Marley X7 Blade Pitch Adjustment
The Marley X7 fan is designed for induced-draft cooling tower applications, offering distinct advantages over other fan designs. Watch this video to learn how to adjust your cooling tower's X7 fan blades.
Regolazione del passo delle pale della ventola della torre di raffreddamento Marley H3
Come si regola il passo delle pale delle pale della ventola Marley H3? Gli ingegneri Marley dimostrano il processo, compresi gli strumenti necessari per completare il lavoro.
Marley Cooling Tower Belt Drive Components
In this video, learn about Marley belt drive components and view a demonstration of belt tensioning and sheave alignment for your cooling tower's belt drive system.
Marley Cooling Tower Hanging Fill Replacement
What's the best way to replace the hanging fill in your cooling tower? Watch a demonstration of quick and easy Marley cooling tower fill replacement here.
Marley MBX Cooling Tower Fill Packs
Robert Swafford from Marley demonstrates the right way to quickly and easily replace your cooling tower's dirty fill with Marley MBX fill packs.
Proof in Performance – Heat Transfer Fill Part 3
What are the benefits of using genuine Marley heat transfer fill? Learn all about it from a Marley expert: (Part 3 of 3).
Proof in Performance – Heat Transfer Fill Part 2
What are the benefits of using genuine Marley heat transfer fill? Learn all about it from a Marley expert: (Part 2 of 3).
Proof In Performance – Heat Transfer Fill Part 1
What are the benefits of using genuine Marley heat transfer fill? Learn all about it from a Marley expert: (Part 1 of 3).
Marley NC Single Bottom Inlet
What are the advantages of the single bottom inlet in a Marley NC cooling tower, and how does it play a part in cooling tower efficiency and cooling tower maintenance?
Allineamento dell'albero motore della torre di raffreddamento Marley
I giunti e gli alberi di trasmissione devono essere robusti, durevoli e allineati correttamente per trasmettere in modo efficiente la potenza dal motore della torre di raffreddamento al cambio. Guarda una dimostrazione di come utilizzare il kit indicatore quadrante Marley per allineare l'albero motore di una torre di raffreddamento Marley qui:
Marley MC Series Coupling Adjustment
If your cooling tower utilizes a Marley MC series coupling, it might need to be occasionally maintained or adjusted. Watch here as we demonstrate how to perform basic maintenance and adjustments on a typical Marley MC series coupling.
Marley Pinion Shaft Oil Seal Replacement
Marley cooling tower gearboxes are equipped with long-life pinion oil seals. If the pinion shaft oil seal on your cooling tower's gearbox has become worn or is leaking, watch here as we demonstrate the best way to replace it.
Interruttore di vibrazione meccanico Marley
Gli interruttori a vibrazione della torre di raffreddamento attivano un allarme e/o spengono l'apparecchiatura quando si verificano vibrazioni eccessive. Guarda qui come un esperto di prodotti Marley dimostra la funzionalità di un interruttore di vibrazione meccanico, incluso come testare tale funzionalità sul campo.
Marley LLC Water Level Control Part 9 – Troubleshooting The Connection Points
Marley LLC Water Level Control systems monitor and adjust the water level in the cooling tower cold water collection basin. Watch our Marley Controls expert as he provides an overview of LLC operation (part 9 of 9: Troubleshooting the Connection Points).
Marley LLC Water Level Control Part 8 – Troubleshooting The Solenoid Valve
Marley LLC Water Level Control systems monitor and adjust the water level in the cooling tower cold water collection basin. Watch our Marley Controls expert as he provides an overview of LLC operation (part 8 of 9: Troubleshooting the Solenoid Valve).
Marley LLC Water Level Control Part 7 – Troubleshooting The Makeup Card
Marley LLC Water Level Control systems monitor and adjust the water level in the cooling tower cold water collection basin. Watch our Marley Controls expert as he provides an overview of LLC operation (part 7 of 9: Testing the Makeup Card).
Marley LLC Water Level Control Part 6 – Troubleshooting The Panel
Marley LLC Water Level Control systems monitor and adjust the water level in the cooling tower cold water collection basin. Watch our Marley Controls expert as he provides an overview of LLC operation (part 6 of 9: Troubleshooting).
Marley LLC Water Level Control Part 5 – Testing
Marley LLC Water Level Control systems monitor and adjust the water level in the cooling tower cold water collection basin. Watch our Marley Controls expert as he provides an overview of LLC operation (part 5 of 9: Control Panel).
Marley LLC Water Level Control Part 4 – Control Panel
Marley LLC Water Level Control systems monitor and adjust the water level in the cooling tower cold water collection basin. Watch our Marley Controls expert as he provides an overview of LLC operation (part 4 of 9: Control Panel).
Marley LLC Water Level Control Part 3 – Start Up
Marley LLC Water Level Control systems monitor and adjust the water level in the cooling tower cold water collection basin. Watch our Marley Controls expert as he provides an overview of LLC operation (part 3 of 9: Start-Up).
Marley LLC Water Level Control Part 2 – Installation
Marley LLC Water Level Control systems monitor and adjust the water level in the cooling tower cold water collection basin. Watch our Marley Controls expert as he provides an overview of LLC operation (part 2 of 9: Installation).
Marley LLC Water Level Control Part 1 – Introduction
Marley LLC Water Level Control systems monitor and adjust the water level in the cooling tower cold water collection basin. Watch our Marley Controls expert as he provides an overview of LLC operation (part 1 of 9: Introduction).
Marley Cooling Tower Drift Eliminator
Low drift rates are the primary goal of a drift eliminator. Marley drift eliminator advancements can yield drift rates as low as 0.0005% of design flow rates. This video reviews the advantages of using Marley's newly redesigned drift eliminators.
Marley NC Internal Accessibility
The Marley NC cooling tower's two large access doors provide non-confining, quick visual inspection of cold water basin, internal structure, drift eliminators and mechanical equipment in the plenum area. Take a look:
Expanded Geareducer Cooling Tower Gearbox Line
Marley Series M Geareducers are designed and manufactured to directly replace other OEM gearboxes in cooling towers for power and industrial applications.
NC Everest Cooling Tower Walkthrough
SPX Cooling Technologies embarked on a mission to design and build a cooling tower like no other in the world. Like adventurers climbing Mt. Everest, we knew the challenges yet were driven to achieve something remarkable. Watch here.
Marley Cooling Tower Gearbox Repair Program
Whether you have questions on Geareducer operation and maintenance, need components to perform a repair yourself, or want to send your unit back to us for the highest level of care, SPX has the solution.
Cube Installation
In this video, learn more about the SGS Cube evaporative condenser assembly and installation process.
Marley ClearSky Cooling Tower Plume Abatement
There are many reasons why you might want to reduce your cooling tower's visible plume. Marley ClearSky plume abatement is a fully integrated system that operates more reliably than coil-based systems.
Cooling Tower Lift
Watch as a Marley NC cooling tower is lifted on to a hospital in Overland Park, Kansas.
TDI NC Cooling Tower Installation
Watch as TDI installs Marley NC cooling towers on the Thanksgiving Tower in Dallas, Texas.
Torre di raffreddamento Marley Modular F400
Gli innovativi concetti di costruzione modulare delle torri di raffreddamento di SPX Cooling Tech supportano iniziative di sicurezza, programmi ridotti, meno personale che lavora in loco e altro ancora. Guarda una presentazione della nuova torre di raffreddamento Marley Modular F400 qui:
Marley NC Cooling Tower Overview
The Marley NC Cooling Tower has set the standard for high efficiency and low maintenance since its introduction in 1968. Learn more about cooling tower performance by watching an overview of the Marley NC cooling tower here: