Cooling Tower Video Library
Vorstellung des adiabatischen OlympusV™-Systems
The Marley® and Recold® Adiabatic Series balances the water-saving benefits of an air-cooled heat rejection system with the energy efficiency of a water-cooled solution
Marley® WaterGard™ Kühlturmfilter
WaterGard physically blocks and rejects minerals commonly found in municipal water streams (chlorides, calcium carbonate, silica, etc.), reducing makeup water mineral content and enabling higher operating COC, resulting in reduced volume requirements for both blowdown and supply water.
SPX-Kühlung – Natürlich von innen nach außen
From the outside looking in, this is just a building. A collection of walls, windows and doors. But from the inside, this is a window of opportunity.
Zukunftsorientierte Schule installiert LW-Flüssigkeitskühler
In 2015, Trevor Day School completed a new state-of-the-art vertical campus building in Manhattan’s Upper East Side. The project earned LEED Gold certification and won a 2016 AIA WHV High Honor Award. Part of the building’s sustainability initiatives was the school’s HVAC system. The building would be heated and cooled with a closed-loop “energy pile” geothermal system, one of the first systems of its kind in the U.S. When the system needed to expand its heating/cooling abilities in 2022, the project engineers turned to SPX Cooling Tech for a solution. The team chose to install induced-draft, closed-circuit Marley LW Fluid Coolers for more efficient heat rejection. Marley LW fluid coolers are designed to be installed quickly and offer a small footprint for easier integration into existing systems. These towers are delivered with factory-installed controls, factory wired and tested and are equipped with ultra-efficient, corrosion-resistant copper coils. To reduce the heat of their process fluids, the school would need two LW units. The units were hoisted into position using a crane that reached 200+ ft. into the air to install the fluid coolers onto a newly created platform atop the school’s roof. Installation was completed in a single day and the systems were ready to go just before the beginning of the school year. For more about the LW, and other closed-circuit cooling tower solutions, visit spxcooling.com/fluidcoolers.
Überblick über die SPX Corporation
SPX Corporation is, along with its subsidiaries, a diversified, global supplier of infrastructure equipment with scalable growth platforms in heating, ventilation and air conditioning (HVAC), and detection and measurement. With operations in 15 countries and more than $1 billion in annual revenue, we offer a wide array of highly engineered products with strong brands.
Auswahl aus einem Jahrhundert Marley
Eine kurze Geschichte der Marke Marley und der Marley-Produkte im Laufe unserer 100-jährigen Geschichte.
Marley® BasinGard™ Filterinstallation für NC8400-Türme
Der Marley BasinGard-Filter spart Zeit und Geld, indem er die Reinigung des Warmwasserbeckens eines Kühlturms vereinfacht und Kühlturmkomponenten schützt.
Wir stellen vor: CoolSpec™ Kühlturm-Produktauswahl
CoolSpec™ Selection Software is a new, intuitive tool that compares and selects Marley® and Recold® brand evaporative cooling products - open-circuit and closed-circuit, crossflow and counterflow - cooling towers, fluid coolers and evaporative condensers.
Verdunstungskühltürme im Rechenzentrumsprozess
Die enorme Rechenleistung in Rechenzentren erzeugt Wärme, weshalb eine effiziente Kühlung eine wichtige Anforderung an Gebäudesysteme darstellt. Verdunstungskühltürme sind ein integraler Bestandteil vieler Kühlsysteme für Rechenzentren.
Marley® BasinGard™ Filterinstallation für NC8300-Türme
Der Marley BasinGard-Filter spart Zeit und Geld, indem er die Reinigung des Warmwasserbeckens eines Kühlturms vereinfacht und Kühlturmkomponenten schützt.
Marley® Modularer Kühlturm-Teaser
SPX Cooling Technologies’ innovative modular cooling tower construction concepts support safety initiatives, compressed schedules, fewer working hands on-site and more. Contact your local sales representative to watch the full video and learn more about modular cooling tower options: /rep-search/
Wir stellen vor: den Marley MH Element™ Flüssigkeitskühler
Die beliebte Marley MH Fluid Cooler-Reihe wurde um weitere Modelle erweitert. Der Marley MH Element™ Flüssigkeitskühler mit zusätzlichen Kupferspulen bietet die größte Effizienz pro Stellfläche.
Wir präsentieren den industriellen Verdunstungskondensator von SGS
Wenn Sie Ihren Bedarf an einem hochwertigen industriellen Verdunstungskondensator erfüllen, können Sie sich darauf verlassen, dass der neue industrielle Verdunstungskondensator von SGS präzise konstruiert und sorgfältig hergestellt wird.
Marley NC Everest Kühlturminstallation – Adan Hospital
One of the largest hospitals in Kuwait designed its cooling system with 6 cells of the Marley NC Everest Cooling Tower. With up to 50% greater cooling capacity, the tower cells serve five 1,850-ton chillers and offer higher energy savings, fewer components and lower maintenance costs!
So installieren Sie einen Marley® NC®-Kühlturm, Folge 13: Lüfterzylinder
Marley®-Lüfterzylinder sind entscheidende Komponenten zum Schutz der Lüfterflügel, zur Minimierung von Geräuschen und Vibrationen und zur Ermöglichung einer optimalen Leistung bei allen Kühlturmanwendungen.
Marley FIT Kühlturm-Auswahlsoftware
Our new Marley FIT air delivery selection software takes into consideration the relationship among all cooling tower mechanical system components to recommend a complete system. Air flow is directly proportional to the thermal performance of your cooling tower. Using performance data derived from the SPX Research and Development Center and independently tested and verified, Marley FIT Selection Software facilitates maximum cooling tower performance and maximum value. Get FIT. Register now at www.marleyfit.com.
So installieren Sie einen Marley® NC®-Kühlturm, Folge 12: Gerinne und Wehrtore
Bei NC-Kühltürmen mit mehr als einer Zelle ist eine Verbindungskanalbaugruppe zum Ausgleich und zur Aufrechterhaltung des richtigen Wasserstands zwischen mehreren Sammelbecken eine Option.
So installieren Sie einen Marley® NC®-Kühlturm, Folge 11: Motor außerhalb des Luftstroms
Bei Türmen mit der Option „Motor Outside Airstream“ oder MOA werden der Motor, die Motorhalterung und die Antriebswelle vor Ort installiert und ausgerichtet.
So installieren Sie einen Marley® NC®-Kühlturm, Folge 10: Montage und Installation der Leiter
Wenn Ihr Marley NC-Kühlturm über eine optionale Leiter für den Zugang zum Lüfterdeck verfügt, sehen Sie sich dieses Video an, um eine ordnungsgemäße Installation und Konfiguration sicherzustellen.
So installieren Sie einen Marley® NC®-Kühlturm, Folge 9: Leitplanke für Lufteinlass-Stirnleiter
Wenn Ihr Marley NC-Kühlturm über ein optionales Geländer für eine Lufteinlassleiter (Lamellen) verfügt, sehen Sie sich dieses Video an, um eine ordnungsgemäße Installation und Konfiguration sicherzustellen.
So installieren Sie einen Marley® NC®-Kühlturm, Folge 8: Leitplanke für verkleidete Stirnleiter
Wenn Ihr Marley NC-Kühlturm über ein optionales Geländer für eine verkleidete Frontleiter verfügt, sehen Sie sich dieses Video an, um eine ordnungsgemäße Installation und Konfiguration sicherzustellen.
Marley Kühlturm Advanced Basin Heater (ABH)
Das Marley ABH-Bedienfeld (Advanced Basin Heater) steuert den Ein-/Aus-Betrieb der Kaltwasserbeckenheizung(en) und verhindert das Einfrieren in kalten Umgebungen. Sehen Sie sich an, wie ein Marley-Experte die Funktionen, Vorteile und den Betrieb des Marley Advanced Basin Heater-Kühlturm-Bedienfelds erläutert.
So installieren Sie einen Marley® NC®-Kühlturm, Folge 7: HC-Ventile
Wenn Ihr Marley NC-Kühlturm optionale Horizontalsteuerventile (HC) enthält, sehen Sie sich dieses Video an, um eine ordnungsgemäße Installation und Konfiguration sicherzustellen.
So installieren Sie einen Marley® NC®-Kühlturm, Folge 6: Lüfterschutz
Befolgen Sie diese Richtlinien, um den Vorgang zu beschleunigen und die korrekte Platzierung des Lüfterschutzes an Ihrem Marley NC-Kühlturm sicherzustellen.
So installieren Sie einen Marley® NC® Kühlturm, Folge 5: Modulare Tipps und Tricks
Um modulare NC-Kühltürme richtig zusammenzubauen und zu installieren, befolgen Sie diese Richtlinien, um häufige Fehler zu vermeiden und den Installationsprozess des Kühlturms zu beschleunigen.
So installieren Sie einen Marley® NC®-Kühlturm, Folge 4: Hebemodule
Befolgen Sie diese einfachen Heberichtlinien, und der gesamte Vorgang zum Heben Ihres Marley NC-Kühlturms an seinen Platz verläuft reibungslos und effizient.
So installieren Sie einen Marley® NC® Kühlturm, Folge 3: Erforderliche Hardware
Um einen Marley NC-Kühlturm richtig zusammenzubauen und zu installieren, muss Ihr Team mit einigen grundlegenden Werkzeugen ausgestattet sein und Sie sollten auch mit einigen grundlegenden Geräten und Verfahren vertraut sein.
So installieren Sie einen Marley® NC® Kühlturm, Folge 2: Installationsanweisungen und Zeichnungen
Das Marley NC-Literaturpaket enthält Ihre Installationsanweisungen, Stücklisten und Installationszeichnungen für alle Standard- und optionalen Komponenten des NC-Kühlturms.
So installieren Sie einen Marley NC-Kühlturm, Folge 1: Standortvorbereitung, Ankunft des Turms und Entladen
Befolgen Sie diese einfachen Richtlinien, dann verläuft der gesamte Prozess für die Ankunft und Entladung Ihres NC-Kühlturms reibungslos und effizient.
Testanlage für Marley-Kühlturmventilatoren
Seit über zwei Jahrzehnten wird jeder Kühlturmventilator von Marley in dieser Modellventilator-Testzelle auf seine Leistung im Feldbetrieb genau geprüft. Hier erhalten Sie einen Einblick:
Marley DT Flüssigkeitskühler
Schauen Sie sich den Marley DT Fluid Cooler an, jetzt mit einer neuen Rippenspulenoption für erweiterte Trockenkapazität und Wärmeleistung!
Marley® NC® Kühlturmserie – Größen-/Kapazitätsvergleich
Wie groß ist ein Marley NC Everest Kühlturm im Vergleich zu anderen Marley NC Kühlturmmodellen? Sehen Sie sich die Unterschiede zwischen den Kühltürmen Marley NC8407, Marley NC8414 und Marley NC8422 an!
Querstrom- vs. Gegenstrom-Kühltürme
Was ist der Unterschied zwischen einem Querstrom- und einem Gegenstromkühlturm? SPX Cooling Tech zeigt die Unterschiede und Vorteile der einzelnen Bauformen.
Marley® NC Everest® Kühlturmbaugruppe
Sehen Sie zu, wie der allererste Marley® NC Everest®-Kühlturm im Forschungs- und Entwicklungszentrum von SPX zusammengebaut wird.
Marley® HC Durchflussregelventile für Kühltürme
Marley® HC-Ventile bieten eine niedrige Austrittsgeschwindigkeit und begrenzen Spritzer, was zu einem geringen Druckabfall führt. Erfahren Sie hier mehr darüber, wie sie die Leistung Ihres Kühlturms beeinflussen:
Marley® Quadraflow Wartung
Das einzigartige, kompakte Design des QuadraFlow wird durch seine Leistung, Wartungsfreundlichkeit und Zuverlässigkeit ergänzt. Sehen Sie sich an, wie ein Marley-Experte die Vorteile und die ordnungsgemäße Wartung des Marley Quadraflow-Kühlturms erläutert.
Reparatur des Kühlturms im Kraftwerk Didcot B
Follow our Time Lapse video as SPX repairs Didcot B Power Station's cooling tower cells to their original design following an unfortunate fire that severely damaged more than three cells.
Ist die Füllung meines Kühlturms verschmutzt?
Woher wissen Sie, wann es Zeit ist, den Kühlturmfüllkörper auszutauschen? Sehen Sie sich an, wie ein Marley-Experte erklärt, wie Sie den Unterschied zwischen einem Kühlturmfüllkörper mit normaler Kalkablagerung und einem verstopften Füllkörper erkennen, der gewartet werden muss.
Marley® Kühlturm-Integrallamellen
Was sind integrierte Lamellen und welchen Unterschied machen sie für den Betrieb, die Kosten und die Leistung Ihres Kühlturms? Sehen Sie sich an, wie wir die Vorteile besprechen.
301L vs. 304 Edelstahl
Die Stahlsorte, die beim Bau Ihres Kühlturms verwendet wird, macht einen Unterschied. In diesem Video besprechen wir die Vorteile der Verwendung von 301L-Edelstahl in Ihrem Marley-Kühlturm.
Marley® Geareducer® Kühlturm-Getriebeölwechsel
Wie wechsle ich das Getriebeöl meines Kühlturms? Der Ölwechsel in Ihrem Marley Geareducer-Kühlturmgetriebe ist unkompliziert – sehen Sie sich in diesem Video die Demonstration durch einen Marley-Experten an.
Kühlturm-Zahnradantriebe vs. Riemenantriebe
Einige Kühltürme treiben ihre Ventilatoren mit Riemenantrieben an, andere verwenden Zahnradantriebe. Aber was ist für Ihre Anwendung besser? In diesem Video besprechen wir die Vorteile der Verwendung eines Marley Geareducer-Zahnradantriebs gegenüber einem Riemenantrieb in Ihrem Kühlturm.
Marley NCWD Kühlturmlift
Der NCWD ist ein innovativer, patentierter, fabrikmontierter Hybrid-Kühlturm, der speziell zur Abgasreduzierung entwickelt wurde. Sehen Sie, wie dieser NCWD in London, England, angehoben wird.
Marley MBX EZ Pack Kühlturmfüllung
Das bauunternehmerfreundliche Design der MBX EZ Pack-Füllung ermöglicht eine schnelle und einfache Installation, ohne dass größere Turmmodifikationen erforderlich sind.
Marley MD Everest Kühlturmbaugruppe
Der MD Everest Kühlturm eignet sich hervorragend für Anwendungen mit höherem Kühlbedarf, darunter Rechenzentren, Fernwärmekomplexe, Gesundheitswissenschaftscampus und Industriekomplexe. Sehen Sie in diesem Video, wie ein neuer modularer Marley MD Everest Kühlturm zusammengebaut wird.
Installation des Marley® M-Serie Geareducer®
Als die Getriebe dieses Kunden anfingen zu vibrieren und Getriebeschäden auftraten, rief er Marley zur Verstärkung. Sehen Sie in diesem Video, wie einfach die alten Getriebe durch Marley-Getriebe ersetzt wurden.
Marley® Lufteinlasssiebe für Kühltürme
Wenn sich in Ihrem Kühlturm Ablagerungen ansammeln oder die Füllung verstopft, sind die Lufteinlasssiebe von Marley eine Lösung. Sehen Sie sich an, wie wir die Vorteile der Verwendung von Lufteinlasssieben an Ihrem Kühlturm besprechen.
Marley Parts Vodcast 1 von 3: Geareducer
Jerome Jennings von Marley / SPX Cooling Tech. erklärt die Vorteile der Verwendung eines Original-Marley Geareducer-Getriebes (Marley Parts Vodcast, Teil 1 von 3).
Marley Parts Vodcast 2 von 3: Antriebswellen
Jerome Jennings von Marley / SPX Cooling Technologies erläutert die Vorteile der Verwendung einer Original-Antriebswelle von Marley (Marley Parts Vodcast, Teil 2 von 3).
Marley Parts Vodcast 3 von 3: Lüfterblätter
Jerome Jennings von Marley / SPX Cooling Technologies erläutert die Vorteile der Verwendung von Original-Lüfterblättern von Marley (Marley Parts Vodcast, Teil 3 von 3).
Marley Kühlturmlagerschmierung
It's important to properly maintain your Marley cooling tower bearings. Watch as a Marley expert provides some helpful tips for making bearing lubrication easy.
Übersicht über das Marley NS Kühlturm-Sprühsystem
Marley NS-Gegenstromdüsen sorgen für eine gleichmäßige Wasserverteilung über einen weiten Betriebswasserdruckbereich und NS-Gegenstromdüsen haben keine Innenteile oder engen Durchgänge, die durch Schmutz verstopft werden können.
Umbau und Reparatur von Marley Geareducer
Whether you have questions on Marley Geareducer cooling tower gearbox operation and maintenance, need components to perform a repair yourself, or want to send your unit back to us for the highest level of care, SPX has the solution.
Marley ST Düsen- und Bechersystem
Das Marley Spiral Target Düsen- und Bechersystem ist eine spritzgegossene Polypropyleneinheit, die aus zwei Teilen besteht – dem Hauptkörper mit integriertem Zieldiffusor und einem aufsteckbaren Einsatz oder einer Düsenkappe. Klicken Sie hier, um mehr zu erfahren.
Marley MH Flüssigkeitskühler
Die beliebte Marley MH Fluid Cooler-Reihe wurde um zusätzliche Modelle erweitert, die alle mit Kupferspulen für eine höhere Wärmekapazität ausgestattet werden können. Sehen Sie sich hier eine kurze Produktübersicht an.
Mechanisches Schwimmersystem für Marley-Kühltürme
What are the advantages to a Marley mechanical cooling tower float system? Why would your cooling tower benefit from a float system? Learn more by watching.
Übersicht über den Kühlturm von Marley MD
Der Marley MD ist ein werkseitig montierter Gegenstromkühlturm. Für viele HVAC- und Leichtindustrieanwendungen erfordert diese Konstruktion weniger Stellfläche und bietet mehr Flexibilität bei der Aufstellung als ein vergleichbarer Querstromkühlturm.
Übersicht über das Marley Geareducer®-Getriebe
Die Zuverlässigkeit des Geareducer beruht auf mehr als 100.000 Einheiten Erfahrung und auf Marleys Aufmerksamkeit für anspruchsvolle Qualitätsstandards bei Design und Herstellung. Heute wird jeder Marley Geareducer in unserem Werk unter Last getestet. Dann wird er vor dem Versand überprüft und eingestellt.
Wartung des Marley-Kühlturms
Die Diagnose von Wartungsproblemen beginnt oft mit der Inspektion mechanischer Geräte und Komponenten, die einem Verschleiß unterliegen – beispielsweise Motoren, Getriebe oder Riemenantriebe.
Marley Kühlturm-Leistungsmotor
Kühlturmmotoren in Marley-Produkten werden gemäß NEMA-Standards gebaut und sind so konstruiert, dass sie den heißen, feuchten Bedingungen in Kühltürmen standhalten. Um eine lange Lebensdauer zu gewährleisten, ist das Innere des Motors zusätzlich lüftergekühlt und mit Epoxidharz beschichtet, um maximalen Schutz vor Hitze, Feuchtigkeit und Korrosion zu gewährleisten.
Marley Kühlturm HC Durchflussregelventil
Die Körperproportionen des HC-Ventils und die Anordnung der Innenteile sorgen für eine niedrige Austrittsgeschwindigkeit und begrenzen Spritzer, was zu einem geringen Druckabfall führt. Sehen Sie sich das Video an, um mehr über die Funktionsweise des HC-Ventils zu erfahren.
Einstellung der extrem leisen Lüfterflügelneigung
The Ultra Quiet fan is designed for HVAC cooling tower applications where very low sound is a necessity. Here's a demonstration on how to adjust the blade pitch on your cooling tower's Ultra Quiet Fan.
Marley X7 Rotorblatt-Neigungseinstellung
Der Marley X7-Lüfter ist für Saugzugkühlturmanwendungen konzipiert und bietet deutliche Vorteile gegenüber anderen Lüfterkonstruktionen. Sehen Sie sich dieses Video an, um zu erfahren, wie Sie die X7-Lüfterblätter Ihres Kühlturms einstellen.
Neigungsverstellung der Marley H3 Kühlturm-Lüfterblätter
Wie stellen Sie den Blattwinkel an den Flügeln Ihres Marley H3-Ventilators ein? Die Techniker von Marley demonstrieren Ihnen den Vorgang und zeigen Ihnen, welche Werkzeuge Sie dafür benötigen.
Marley Kühlturm-Riemenantriebskomponenten
In this video, learn about Marley belt drive components and view a demonstration of belt tensioning and sheave alignment for your cooling tower's belt drive system.
Austausch der hängenden Füllung des Marley-Kühlturms
What's the best way to replace the hanging fill in your cooling tower? Watch a demonstration of quick and easy Marley cooling tower fill replacement here.
Marley MBX Kühlturm-Füllpakete
Robert Swafford from Marley demonstrates the right way to quickly and easily replace your cooling tower's dirty fill with Marley MBX fill packs.
Leistungsnachweis – Wärmeübertragungsfüllung Teil 3
Welche Vorteile bietet die Verwendung von Original-Wärmeübertragungsfüllung von Marley? Erfahren Sie alles darüber von einem Marley-Experten: (Teil 3 von 3).
Leistungsnachweis – Wärmeübertragungsfüllung Teil 2
Welche Vorteile bietet die Verwendung von Original-Wärmeübertragungsfüllung von Marley? Erfahren Sie alles darüber von einem Marley-Experten: (Teil 2 von 3).
Leistungsnachweis – Wärmeübertragungsfüllung Teil 1
Welche Vorteile bietet die Verwendung von Original-Wärmeübertragungsfüllung von Marley? Erfahren Sie alles darüber von einem Marley-Experten: (Teil 1 von 3).
Marley NC Einzelbodeneinlass
Welche Vorteile bietet der einzelne Bodeneinlass in einem Marley NC-Kühlturm und welche Rolle spielt er für die Effizienz und Wartung des Kühlturms?
Ausrichtung der Antriebswelle eines Marley-Kühlturms
Kupplungen und Antriebswellen müssen stark, langlebig und richtig ausgerichtet sein, um die Kraft effizient vom Kühlturmmotor auf das Getriebe zu übertragen. Sehen Sie sich hier eine Demonstration an, wie Sie mit dem Marley-Messuhr-Kit eine Marley-Kühlturm-Antriebswelle ausrichten können:
Kupplungseinstellung der Marley MC-Serie
Wenn Ihr Kühlturm eine Kupplung der Marley MC-Serie verwendet, muss diese möglicherweise gelegentlich gewartet oder eingestellt werden. Sehen Sie sich hier an, wie wir grundlegende Wartungs- und Einstellungsarbeiten an einer typischen Kupplung der Marley MC-Serie durchführen.
Austausch der Ritzelwellen-Öldichtung von Marley
Marley cooling tower gearboxes are equipped with long-life pinion oil seals. If the pinion shaft oil seal on your cooling tower's gearbox has become worn or is leaking, watch here as we demonstrate the best way to replace it.
Mechanischer Vibrationsschalter von Marley
Vibrationsschalter für Kühltürme lösen einen Alarm aus und/oder schalten das Gerät ab, wenn übermäßige Vibrationen auftreten. Sehen Sie hier, wie ein Marley-Produktexperte die Funktionsweise eines mechanischen Vibrationsschalters demonstriert und zeigt, wie diese Funktion vor Ort getestet werden kann.
Marley LLC Wasserstandsregelung Teil 9 – Fehlerbehebung an den Anschlusspunkten
Marley LLC-Wasserstandskontrollsysteme überwachen und regeln den Wasserstand im Kaltwassersammelbecken des Kühlturms. Sehen Sie sich an, wie unser Marley Controls-Experte einen Überblick über den LLC-Betrieb gibt (Teil 9 von 9: Fehlerbehebung an den Verbindungspunkten).
Marley LLC Wasserstandsregelung Teil 8 – Fehlerbehebung beim Magnetventil
Marley LLC-Wasserstandskontrollsysteme überwachen und regeln den Wasserstand im Kaltwassersammelbecken des Kühlturms. Sehen Sie sich an, wie unser Marley Controls-Experte einen Überblick über den LLC-Betrieb gibt (Teil 8 von 9: Fehlerbehebung beim Magnetventil).
Marley LLC Wasserstandsregelung Teil 7 – Fehlerbehebung bei der Makeup-Karte
Marley LLC-Wasserstandskontrollsysteme überwachen und regeln den Wasserstand im Kaltwassersammelbecken des Kühlturms. Sehen Sie sich an, wie unser Marley Controls-Experte einen Überblick über den LLC-Betrieb gibt (Teil 7 von 9: Testen der Makeup-Karte).
Marley LLC Wasserstandsregelung Teil 6 – Fehlerbehebung beim Panel
Marley LLC-Wasserstandskontrollsysteme überwachen und regeln den Wasserstand im Kaltwassersammelbecken des Kühlturms. Sehen Sie sich an, wie unser Marley Controls-Experte einen Überblick über den LLC-Betrieb gibt (Teil 6 von 9: Fehlerbehebung).
Marley LLC Wasserstandsregelung Teil 5 – Testen
Marley LLC-Wasserstandskontrollsysteme überwachen und regeln den Wasserstand im Kaltwassersammelbecken des Kühlturms. Sehen Sie sich an, wie unser Marley Controls-Experte einen Überblick über den LLC-Betrieb gibt (Teil 5 von 9: Bedienfeld).
Marley LLC Wasserstandsregelung Teil 4 – Bedienfeld
Marley LLC-Wasserstandskontrollsysteme überwachen und regeln den Wasserstand im Kaltwassersammelbecken des Kühlturms. Sehen Sie sich an, wie unser Marley Controls-Experte einen Überblick über den LLC-Betrieb gibt (Teil 4 von 9: Bedienfeld).
Marley LLC Wasserstandsregelung Teil 3 – Inbetriebnahme
Marley LLC-Wasserstandskontrollsysteme überwachen und regeln den Wasserstand im Kaltwassersammelbecken des Kühlturms. Sehen Sie sich an, wie unser Marley Controls-Experte einen Überblick über den LLC-Betrieb gibt (Teil 3 von 9: Inbetriebnahme).
Marley LLC Wasserstandsregelung Teil 2 – Installation
Marley LLC-Wasserstandskontrollsysteme überwachen und regeln den Wasserstand im Kaltwassersammelbecken des Kühlturms. Sehen Sie sich an, wie unser Marley Controls-Experte einen Überblick über den LLC-Betrieb gibt (Teil 2 von 9: Installation).
Marley LLC Wasserstandsregelung Teil 1 – Einführung
Marley LLC-Wasserstandskontrollsysteme überwachen und regeln den Wasserstand im Kaltwassersammelbecken des Kühlturms. Sehen Sie sich an, wie unser Marley Controls-Experte einen Überblick über den LLC-Betrieb gibt (Teil 1 von 9: Einführung).
Marley Kühlturm-Tropfenabscheider
Low drift rates are the primary goal of a drift eliminator. Marley drift eliminator advancements can yield drift rates as low as 0.0005% of design flow rates. This video reviews the advantages of using Marley's newly redesigned drift eliminators.
Interne Zugänglichkeit in Marley, NC
The Marley NC cooling tower's two large access doors provide non-confining, quick visual inspection of cold water basin, internal structure, drift eliminators and mechanical equipment in the plenum area. Take a look:
Erweiterte Geareducer-Kühlturmgetriebelinie
Die Geareducer der Marley-Serie M sind so konzipiert und hergestellt, dass sie andere OEM-Getriebe in Kühltürmen für Energie- und Industrieanwendungen direkt ersetzen können.
NC Everest Kühlturm - Komplettlösung
SPX Cooling Technologies hat sich zum Ziel gesetzt, einen Kühlturm zu entwerfen und zu bauen, der seinesgleichen auf der Welt sucht. Wie Abenteurer, die den Mount Everest besteigen, waren wir uns der Herausforderungen bewusst und wollten dennoch etwas Außergewöhnliches erreichen. Sehen Sie es sich hier an.
Marley Kühlturm-Getriebe-Reparaturprogramm
Ob Sie Fragen zu Betrieb und Wartung des Geareducer haben, Komponenten benötigen, um selbst eine Reparatur durchzuführen, oder Ihr Gerät zur bestmöglichen Betreuung an uns zurücksenden möchten, SPX hat die Lösung.
Cube Installation
In this video, learn more about the SGS Cube evaporative condenser assembly and installation process.
Marley ClearSky Kühlturm-Abgasreinigung
There are many reasons why you might want to reduce your cooling tower's visible plume. Marley ClearSky plume abatement is a fully integrated system that operates more reliably than coil-based systems.
Kühlturmlift
Sehen Sie zu, wie ein Kühlturm von Marley NC auf ein Krankenhaus in Overland Park, Kansas, gehoben wird.
TDI NC Cooling Tower Installation
Watch as TDI installs Marley NC cooling towers on the Thanksgiving Tower in Dallas, Texas.
Marley Modular F400 Kühlturm
Die innovativen modularen Kühlturm-Konstruktionskonzepte von SPX Cooling Tech unterstützen Sicherheitsinitiativen, verkürzte Zeitpläne, weniger Arbeitskräfte vor Ort und mehr. Sehen Sie sich hier eine Präsentation des neuen modularen Kühlturms Marley F400 an:
Übersicht über den Kühlturm von Marley, NC
Der Marley NC-Kühlturm hat seit seiner Einführung im Jahr 1968 den Standard für hohe Effizienz und geringen Wartungsaufwand gesetzt. Erfahren Sie mehr über die Leistung von Kühltürmen, indem Sie sich hier eine Übersicht über den Marley NC-Kühlturm ansehen: