Recycled Material

We have a strong commitment to using recycled materials in our products. At the end of a product’s life, many of the materials used in manufacturing and construction can be recycled.

Marley NC cooling towers, for example, are composed of about 70 percent recycled material when the structure is manufactured out of stainless steel or 29 percent when manufactured out of galvanized steel.

Our cooling towers frequently use gearboxes containing oil for lubrication and cooling. The Marley System 5 Geareducer has been designed to operate five years between oil changes which greatly reduces the amount of oil that needs to be recycled.

LEED Credits
It is important to note that LEED, the US national standard for green buildings, does not include large mechanical equipment such as elevators and air-conditioning equipment, which includes cooling towers, as a part of the recycled or regional sourced materials calculations.

下载:

英国杂志 ACR News 发表了我们的问答文章,调查工程师和设计专家,解释冷却塔如何为 LEED 项目和其他可持续发展计划的成功做出贡献。

zh_CN