Operating Cooling Towers in Freezing Weather
首页 / 图书馆 / Operating Cooling Towers in Freezing Weather
Operating Cooling Towers in Freezing Weather
白皮书
A properly designed cooling tower promotes the maximum possible contact between air and water—and does so for the maximum possible time period. This effort on the part of the designer results in an efficiency which, although greatly appreciated in the summertime, has the capability to produce performance-degrading ice formations during winter operation.可用的文档语言