Expert Opinion Whitepapers


Test

How to Conserve Water in Evaporative Cooling Towers
Expert Opinion Whitepapers | News

When it comes to heat rejection in mechanical systems, evaporative cooling towers (or water-cooled solutions) use less power than air-cooled options, making them more energy-efficient.
When it comes to heat rejection in mechanical systems, evaporative cooling towers (or water-cooled solutions) use less power than air-cooled options, making them more energy-efficient. Cooling towers can use significant amounts of water because they reject heat by...
Test

Cooling Tower Reconstruction
Expert Opinion Whitepapers | News

After many years of operation, cooling towers may require more than routine maintenance and component replacement to achieve the thermal performance necessary to support plant processes. In addition to achieving proper thermal performance, plants also must address the...
Test
The next generation of factory-assembled cooling towers can be delivered up to 60 percent faster than field-erected towers and installed 80 percent faster. Recent developments in factory-assembled cooling tower technology are increasing the applications for...
Test

How FM APPROVED Cooling Towers Help Reduce Risks
Expert Opinion Whitepapers | News

When water flow is temporarily suspended, as in the event of a fire, some cooling towers that contain combustible materials and dry areas may be at risk. Some organizations practice loss prevention by considering an FM APPROVED cooling tower to potentially reduce...
Test

Cooling Solutions for Chemical Process Plants
Expert Opinion Whitepapers | News

Heavy industrial applications such as manufacturing, chemical processing and oil-and-gas refining use cooling towers and other equipment to cool the water integral to their operations. As environmental regulations and challenging market conditions place higher demands...
Test
Gearboxes are used as speed reducers to slow rotational speed from the incoming motor to the outgoing fan of a cooling tower. Industries that require process heat rejection often use field-erected cooling towers to keep pace with their heat load. Cooling towers have...
en_US