Marley NC8400 Revit Files
The Revit product family for the Marley NC8400 provides the basic geometry and typical pipe connections for each unit size of the product line. The product family covers the steel cased NC8400 cooling tower, but not the fiberglass version. The product family is compatible with Revit version 2009 and later.
Inlet Connections
The standard dual inlet connections are included in this product family. The inlet size is automatically set according to the unit size selected. The piping connected to these inlets should supply equal water flow to both inlets. The horizontal control (HC) valves option and the Marley single inlet option are not included in this model.
Outlet Connections
Three types of outlet connections are included in this product family: side outlet face A, side outlet face C, and bottom outlet. Only one of the outlets should be connected; the other two should be ignored or deleted. After the inlet water flows are defined, the outlet water flow and outlet diameters are calculated automatically. The NC8400 has an option for a sump outlet which is not included in this model.
Optional Accessories
The following optional accessories are selectable parameters in the Structural category:
- Guardrail with Ladder on Face A
- Guardrail with Ladder on Face B
- Guardrail with Ladder on Face C
- Guardrail with Ladder on Face D
- Access Door Platform on Face A
- Access Door Platform on Face C
The ladder options for faces A and C cannot be used in combination with the ladder options for faces B and D. The access door platform cannot be used on the same face as a side outlet. Other optional accessories may alter or prevent the use of these options, and some optional components can increase the size of the unit.
Multiple Cells
Multiple instances of the NC8400 product family may be inserted into the Revit model for installations having multiple cells. They must all be oriented in the same direction and positioned so the access doors on faces A and C are facing each other. There is a standard spacing between cells and an alternate wider spacing to permit the fan motor to be mounted outside the airstream. Ladders and Access Door Platforms cannot be used between cells.
| Center-to-Center Spacing | ||
| Unit Size | Standard | Wide |
| NC8401 | 81.75" (2076mm) | 114" (2896mm) |
| NC8402 | 104.25" (2648mm) | 136.5" (3467mm) |
| NC8403 | 104.25" (2648mm) | 136.5" (3467mm) |
| NC8405 | 122.25" (3105mm) | 154.5" (3924mm) |
| NC8407 | 146.25" (3715mm) | 178.5" (3434mm) |
| NC8409 | 170.25" (4324mm) | 202.5" (5144mm) |
| NC8411 | 146.25" (3715mm) | 178.5" (3434mm) |
| NC8412 | 170.25" (4324mm) | 202.5" (5144mm) |
| NC8413 | 146.25" (3715mm) | 178.5" (3434mm) |
| NC8414 | 170.25" (4324mm) | 202.5" (5144mm) |
Clearances
The guardrail, ladder, and access door accessories show the required clearance for these options. Additionally, clearance must be provided at the air inlets and air discharge for adequate air flow. The clearance requirements vary by application, but the air inlet clearance can be approximated as the width of the air inlet for one cell, and the air discharge clearance should be three fan diameters. Also note that vertical enclosures around the cooling tower should not rise above the fan discharge, otherwise air recirculation will impact performance.
Download Revit Files