How To Install A Marley NC Cooling Tower Episode 11: Motor Outside Airstream
On towers with a Motor Outside Airstream, or MOA option, the motor, motor support and driveshaft are installed and aligned on site.
On towers with a Motor Outside Airstream, or MOA option, the motor, motor support and driveshaft are installed and aligned on site.
Marley® BasinGard™ Filter Installation and Replacement
The Marley® BasinGard™ filter saves time and money by simplifying the cleaning of a cooling tower’s hot water basin, and protecting cooling tower components.Marley® Modular Cooling Tower Teaser
SPX Cooling Technologies’ innovative modular cooling tower construction concepts support safety initiatives, compressed schedules, fewer working hands on-site and more. Contact your local sales representative to watch the full video and learn more about modular cooling tower options: https://dev-spx-cooling.pantheonsite.io/rep-search/Introducing The Marley MH Element™ Fluid Cooler
The popular Marley MH Fluid Cooler line has expanded to include additional models. The Marley MH Element™ Fluid Cooler with the addition of copper coils provides the greatest efficiency per footprint.Introducing SGS Industrial Evaporative Condenser
Answering your need for a quality industrial evaporative condenser, count on the new SGS Industrial Evaporative Condenser to be precision engineered and carefully manufactured.Marley NC Everest® Installation – Adan Hospital
One of the largest hospitals in Kuwait designed its cooling system with 6 cells of the Marley® NC Everest® Cooling Tower. With up to 50% greater cooling capacity, the tower cells serve five 1,850-ton chillers and offer higher energy savings, fewer components and lower maintenance costs!How To Install A Marley NC Cooling Tower Episode 13: Fan Cylinder
Marley® fan cylinders are crucial components for protecting fan blades, minimizing sound and vibration, and facilitating optimal performance across all cooling tower applications.Marley FIT Selection Software
Our new Marley FIT air delivery selection software takes into consideration the relationship among all cooling tower mechanical system components to recommend a complete system. Air flow is directly proportional to the thermal performance of your cooling tower. Using performance data derived from the SPX Research and Development Center and independently tested and verified, Marley FIT Selection Software facilitates maximum cooling tower performance and maximum value. Get FIT. Register now at www.marleyfit.com.How To Install A Marley® NC® Cooling Tower Episode 12: Flumes and Weir Gates
On NC cooling towers with more than one cell, an interconnecting flume assembly to equalize and maintain proper water level between multiple collection basins is an option.How To Install A Marley NC Cooling Tower Episode 11: Motor Outside Airstream
On towers with a Motor Outside Airstream, or MOA option, the motor, motor support and driveshaft are installed and aligned on site.How To Install A Marley NC Cooling Tower Episode 10: Ladder Assembly and Installation
If your Marley NC Cooling Tower includes an optional ladder for accessing the fan deck, watch this video to ensure proper installation and configuration.How To Install A Marley NC Cooling Tower Episode 9: Guardrail for Air-Inlet Face Ladder
If your Marley NC Cooling Tower includes an optional guardrail for a air-inlet (louver) face ladder, watch this video to ensure proper installation and configuration.How To Install A Marley NC Cooling Tower Episode 8: Guardrail for Cased Face Ladder
If your Marley NC Cooling Tower includes an optional guardrail for a cased face ladder, watch this video to ensure proper installation and configuration.Marley Advanced Basin Heater (ABH)
Mark Groothuis (Electrical Products Manager) reviews the features, benefits and operation of the Marley® Advanced Basin Heater cooling tower control panel.How To Install A Marley® NC® Cooling Tower Episode 7: HC Valves
If your Marley NC Cooling Tower includes optional Horizontal Control (HC) Valves, watch this video to ensure proper installation and configuration.How To Install A Marley® NC® Cooling Tower Episode 6: Fan Guards
Follow these guidelines to speed the process and ensure correct placement of the fan guard on your Marley NC Cooling Tower.How To Install A Marley® NC® Cooling Tower Episode 5: Modular Tips and Tricks
In order to correctly assemble and install modular NC Cooling Towers, follow these guidelines to avoid common mistakes and speed the cooling tower installation process.How To Install A Marley® NC® Cooling Tower Episode 4: Hoisting Modules
Follow these simple hoisting guidelines and the entire process for hoisting your Marley NC cooling tower into place will be smooth and efficient.How To Install A Marley NC Cooling Tower Episode 3: Necessary Hardware
In order to correctly assemble and install a Marley NC Cooling Tower, your team will need to be prepared with some basic tools, and you should also be aware of some basic equipment and procedures.How To Install A Marley NC Cooling Tower Episode 2: Installation Instructions and Drawings
The Marley NC literature pack includes your installation instructions, bill of materials, and installation drawings for all NC cooling tower’s standard and optional components.How To Install A Marley NC Cooling Tower Episode 1: Site Prep, Tower Arrival and Unloading
Follow these simple guidelines and the entire process for your NC Cooling Tower’s arrival and unloading will be smooth and efficient.Marley Fan Test Facility
For over two decades, every Marley® fan has been accurately verified for field performance in this model fan test cell.Marley DT Fluid Cooler
Take a look at the Marley DT Fluid Cooler, now with a new finned coil option for expanded dry capacity and thermal performance!Marley® NC® Series – Size/Capacity Comparison
Just how big is a Marley NC Everest cooling tower compared to other Marley NC cooling tower models? Take a look at the difference in dimensions and capacity between Marley NC8407, the Marley NC8414 and the Marley NC8422 cooling towers!Crossflow Vs. Counterflow Cooling Towers
Spencer Kaufman with SPX Cooling Technologies, Inc. demonstrates the differences between crossflow and counterflow cooling towers.Marley® NC Everest® Assembly
Watch as the very first Marley® NC Everest® cooling tower is assembled at the SPX Research and Development Center.Marley® HC Flow Control Valves
Marley® HC valves provide a low discharge velocity and confine splash, resulting in low pressure drop.Marley® Quadraflow Maintenance
Mitch Case discusses the advantages and proper maintenance of the Marley® Quadraflow cooling tower.Is My Cooling Tower Fill Dirty?
Mitch Case discusses how to tell the difference cooling tower fill with normal scale build-up and clogged fill that needs maintenance.Didcot B Power Station Repair
Follow our Time Lapse video as SPX repairs Didcot B Power Station's cooling tower cells to their original design following an unfortunate fire that severely damaged more than three cells.Marley® Integral Louvers
Ryan Miller with SPX Cooling Technologies discusses the advantages of using Marley® Integral Louvers in your cooling tower.301L vs 304 Stainless Steel
Joe Evans with SPX Cooling Technologies discusses the advantages of using 301L stainless steel in your Marley® cooling tower.Marley® Geareducer® Gearbox Oil Change
Jerome Jennings walks through the process of changing the oil in your Marley® Geareducer® cooling tower gearbox.Cooling Tower Gear Drives Vs. Belt Drives
Jerome Jennings discusses the benefits of using a Marley® Geareducer® gear drive over a belt drive in your cooling tower.Marley NCWD Cooling Tower Lift
The NCWD is an innovative, patented factory assembled hybrid cooling tower designed specifically for plume reduction. Watch as this NCWD is lifted in London, England.Marley MBX EZ Pack Fill
The MBX EZ Pack fill's contractor-friendly fill design makes installation fast and easy without requiring major tower modifications.Marley MD Everest Assembly
Watch as the new Marley MD Everest modular cooling tower is assembled. For more information, visit https://dev-spx-cooling.pantheonsite.io/products/marley-md-everest.Marley® M Series Geareducer® Installation
The new Marley® M Series Geareducer® Gear Drive: Easy Installation; Reliable Performance.Marley® Air Inlet Screens
Mitch Case with SPX Cooling Technologies discusses the advantages of using Marley air inlet screens on your cooling tower.Marley Parts Vodcast 3 of 3: Fan Blades
Jerome Jennings from Marley / SPX Cooling Technologies explains the benefits of using genuine Marley Fan Blades (Marley Parts Vodcast Part 3 of 3).Marley Parts Vodcast 1 of 3: Geareducer
Jerome Jennings from Marley / SPX Cooling Technologies explains the benefits of using a genuine Marley Geareducer gearbox (Marley Parts Vodcast Part 1 of 3).Marley Parts Vodcast 2 of 3: Driveshafts
Jerome Jennings from Marley / SPX Cooling Technologies explains the benefits of using a genuine Marley driveshaft (Marley Parts Vodcast Part 2 of 3).Marley Cooling Tower Bearing Lubrication
Jerome Jennings, Product Manager for SPX Cooling Technologies, Inc., explains the importance of properly maintaining Marley cooling tower bearings and provides some helpful tips for making bearing lubrication easy.Marley NS Spray System Overview
Jerome Jennings, product manager for SPX Cooling Technologies Inc, discusses the advantages of the Marley NS Spray System for field erected cooling towers.Marley Geareducer Rebuild and Repair
Whether you have questions on Marley Geareducer operation and maintenance, need components to perform a repair yourself, or want to send your unit back to us for the highest level of care, SPX has the solution.Marley ST Nozzle and Cup System
Rob Negless, Sr. Engineer with SPX Cooling Technologies, discusses the benefits of the Marley ST Nozzle and Cup system.Marley MH Fluid Cooler
Ryan Miller, Regional Sales Manager for SPX Cooling Technologies, provides an overview of the Marley MH Fluid Cooler.Marley Mechanical Float System
Mitch Case with SPX Cooling Technologies Discusses the Marley Mechanical Float System.Marley MD Tower Overview
Mitch Case with SPX Cooling Technologies provides an overview of the features of the Marley MD Cooling Tower.Marley Cooling Tower Duty Motor
Ryan Miller with SPX Cooling Technologies talks about Weg Duty Motors for Marley cooling towers.Marley Geareducer® Gearbox Overview
Mitch Case with SPX Cooling Technologies provides an overview of the Marley Geareducer gearbox.Marley Cooling Tower Maintenance
Mitch Case from SPX Cooling Technologies discusses mechanical service tips for your Marley cooling tower.Marley HC Flow Control Valve
Robert Swafford, Parts Manager for SPX Cooling Technologies, provides an overview of the operation of the Marley HC Flow Control ValveMarley H3 Fan Blade Pitch Adjustment
Gary Stauffer from Marley demonstrates how to adjust the blade pitch on your Marley H3 fan blades.